The \RESET input (G3) in the OMAPL137 does not contain an internal pull-down or pull-up. The eval schematic for the omapl137 contains a 10k ohm pull-up (page 10, http://support.spectrumdigital.com/boards/evmomapl137/revd/files/EVMOMAPL137_Schematics_RevD.pdf
My question is, would you recommend adding a 10k ohm pull-up resistor (R4) if I have the \RESET input configured as depicted in the attachment? The OMAPL137 IC uses the same +3.3V as the AND gate for power in my board. (Please disregard the unconnected pins in the attachment)