Tool/software: TI-RTOS
Hi there,
I am not using I2C0 on OMAP-L138 board and would like to use it as a internal User-custom interrupt.
I have added the following code in the configuration file:
var hwi8Params = new Hwi.Params();
hwi8Params.instance.name = "hwi8";
hwi8Params.priority = 3;
hwi8Params.eventId = 36;
Program.global.hwi8 = Hwi.create(8, "&data_ready_interrupt", hwi8Params);
and I am setting the interrupt manually.. in one of the timer function as following:
IntEventSet(36);
and the ISR for the interrupt is as follows:
void data_ready_interrupt(void)
{
#ifdef _TMS320C6X
IntEventClear(36);
#else
IntSystemStatusClear(56);
#endif
// Do nothing//
}
I don't see the interrupt reaching in the ISR... Am I settings it up incorrectly??
Thanks.