Other Parts Discussed in Thread: CODECOMPOSER
Hello,
I am trying to boot my custom board with secure OMAP L138 from NAND flash, I perform the following steps:
1. Generate the *.ais file using SecureHexAIS_OMAP-L138.exe to unlock the jTAG,
2. Load it to the board using GenericSecureUartHost.exe,
3. Prepare *.ais file using SecureHexAIS_OMAP-L138.exe based on DSP-hello world program ( infinite loop ),
4. Write the program to NAND flash using NAND_writer, ( and change NAND type to 8-bits width )
5. Run secure_boot_NAND which changes a header to encrypted.
During the last step, the SK_setUserKey( void * ) returns 0x7 value which means that the context is in use. Steps 4 and 5 are run from
CodeComposer 7 using jTAG. The *.ais files are generate with
bootExitType=SECUREWITHSK
BootMode=NONE
ROM ID: d800k008
Silicon Revision 2.1
Thank you for your help,
Best Regerds,
Peter.