Hi,
My customers are using EMIFA to access external Flash.
They are trying to access 16-bit asynchronous memory and have ASIZE set to "1", but problems arise.
The problem is that an address shifted 2 bits right is output.
For example, when trying to access 0x0146, 0x0051 is output from EMA_A [16: 0].
I can agree if it only shifts 1 bit for EMA_BA [1], but I do not know the cause of 2 bit shift.
Are there any ideas on the cause or solution of this problem?
Best Regards,
Miyashiro