Other Parts Discussed in Thread: OMAPL138, CSD
Hi,
We have a custom board on which which are interfacing a Micron MMC (specifically, MTFC4GACAANA-4M IT implementing JEDEC Standard No. 84-B451). We have had this up and working for a couple years now. We have now found that we are unable to obtain any more of these Micron chips, so we found what we believe is a pin for pin compatible device (Micron MTFC4GLGDQ-AIT Z implementing JEDEC A441).
The problem I am seeing is that when we use the new part, I don't seem to get a response from the MMC chip. The SYS/BIOS driver detects it as an MMC, but an IOCTL_START never responds from the chip. We assumed that moving from the 4.51 standard to the 4.41 standard would be fine without any changes to the driver or to our initialization code. Am I missing something, or does someone have any idea where to look for more information regarding the OMAP-L138's compatibility with the older JEDEC standard?
Specifically, we have a small DSP only application which we first load over JTAG during board checkout and which is responsible for programming a Linux kernel to the MMC. From here on out, the ARM core boots from the MMC.
Could we consider a later JEDEC standard to which the OMAP-L138 IP is compatible?
Many thanks in advance for your responses!