Other Parts Discussed in Thread: OMAPL138
Dear All,
Please clarify the doubt about L2 cache memory allocation
In Omapl138 data sheet section 3.5 table 3.4 "Top Level Memory Map" page number 22 it says that "0x0080 0000 0x0083 FFFF 256K DSP L2 RAM" and on same table at page number 24 it says "0x1180 0000 0x1183 FFFF 256K DSP L2 RAM"
http://www.ti.com/lit/ds/symlink/omap-l138.pdf
My questions are below
a) What is the difference between these two locations of same L2 cache
b) Which location to use or we can use both the locations (i.e. 256 k at location 0x0080 0000 and 256 k at location 0x1180 0000)
Regards
Ashish