Other Parts Discussed in Thread: OMAPL138
Hello,
Could you please tell me the USB0 pin connections when {USB0=UNused, USB1=Used}?
From the Table 3-30 in the DS, I would think like the followings:
USB0_DM No Connect
USB0_DP No Connect
USB0_ID No Connect
USB0_VBUS No Connect
USB0_DRVVBUS No Connect
USB0_VDDA33 3.3V
USB0_VDDA18 1.8V
USB0_VDDA12 Internal USB PHY output connected to an external 0.22-uF filter capacitor
USB1_DM Use as USB1 func
USB1_DP Use as USB1 func
USB1_VDDA33 Use as USB1 func
USB1_VDDA18 Use as USB1 func
USB_REFCLKIN Use for USB1 or other peripheral function
USB_CVDD 1.2V