Tool/software: TI-RTOS
Hi there,
I would like to using FATFS module to comms with uSD card from DSP core using SYSBIOS OS.
I have downloaded
SYSBIOS 6.46.5.55
Is there any example to implements this. Thanks.
Regards,
Mitesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Mitesh,
There is an example implementation of using FATFS with uSD on C674x DSP in the Processor SDK RTOS:
processors.wiki.ti.com/.../Processor_SDK_RTOS_MMCSD
processors.wiki.ti.com/.../Processor_SDK_RTOS_FATFS
You can setup the SDK and generate the example inside the PDK using
set SDK_INSTALL_PATH = <Location where SDK is installed> Default is C:\ti set TOOLS_INSTALL_PATH = <Location where CCS is installed> Default is C:\ti cd processor_sdk_rtos_omapl138_4_00_00_04 setupenv.bat cd pdk_omapl13x_1_0_x/packages pdkProjectCreate.bat OMAPL138 all little mmcsd dsp
Hope this helps.
Regards,
Rahul
Hi Rahul,
here is the list of example projects I found under the PDK.
PS C:\ti> cd .\processor_sdk_rtos_omapl138_4_00_00_04\
PS C:\ti\processor_sdk_rtos_omapl138_4_00_00_04> .\setupenv.bat
Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
REQUIRED for xdc release build
Example: set CG_XML_BIN_INSTALL_PATH=C:/ti/cg_xml/bin
Optional parameter not configured : DOXYGEN_INSTALL_PATH
REQUIRED for xdc release build
Example: set DOXYGEN_INSTALL_PATH=C:/ti/Doxygen/doxygen/1.5.1-p1/bin
**************************************************************************
Environment Configuration:
LIMIT_SOCS : omapl138
LIMIT_BOARDS : lcdkOMAPL138
PDK_INSTALL_PATH : /ti/PDK_OM~2/packages
C6X_GEN_INSTALL_PATH : C:/ti/ti-cgt-c6000_8.1.3
TOOLCHAIN_PATH_GCC : C:/ti/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_A15 : C:/ti/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_A8 : C:/ti/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_A9 : C:/ti/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_M4 : C:/ti/ti-cgt-arm_16.9.2.LTS
TOOLCHAIN_PATH_Arm9 : C:/ti/ti-cgt-arm_16.9.2.LTS
TOOLCHAIN_PATH_EVE : C:/ti/arp32_1.0.8
CL_PRU_INSTALL_PATH : C:/ti/ti-cgt-pru_2.1.5
UTILS_INSTALL_DIR : C:/ti/xdctools_3_32_01_22_core/bin
FPULIB_PATH : C:/ti/gcc-arm-none-eabi-4_9-2015q3/lib/gcc/arm-none-eabi/4.9.3/fpu
CROSS_TOOL_PRFX : arm-none-eabi-
XDC_INSTALL_PATH : C:/ti/xdctools_3_32_01_22_core
BIOS_INSTALL_PATH : C:/ti/bios_6_46_05_55
IPC_INSTALL_PATH : C:/ti/ipc_3_46_00_02
EDMA3LLD_BIOS6_INSTALLDIR : C:/ti/edma3_lld_2_12_04_28
NDK_INSTALL_PATH : C:/ti/ndk_2_25_01_11
IMGLIB_INSTALL_PATH : C:/ti/imglib_c674x_3_1_1_0
DSPLIB_INSTALL_PATH : C:/ti/dsplib_c674x_3_4_0_0
MATHLIB_INSTALL_PATH : C:/ti/mathlib_c674x_3_1_1_0
UIA_INSTALL_PATH : C:/ti/uia_2_00_06_52
IPC_PLATFORM: OMAPL138
IPC_ALT_PLATFORM:
PROC_SDK_INSTALL_PATH : C:/ti/processor_sdk_rtos_omapl138_4_00_00_04
**************************************************************************
Changing to short name to support directory names containing spaces
current directory: C:/ti/processor_sdk_rtos_omapl138_4_00_00_04
PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
**************************************************************************
PS C:\ti\processor_sdk_rtos_omapl138_4_00_00_04> cd ..
PS C:\ti> cd .\pdk_OMAPL138_1_01_00_02\packages\
PS C:\ti\pdk_OMAPL138_1_01_00_02\packages> C:\ti\pdk_OMAPL138_1_01_00_02\packages\ti\scripts\pdkProjectCreate.bat OMAPL1
38 all little mmcsd dsp
The system cannot find the path specified.
*****************************************************************************
Detecting UnitTest Projects in PDK and importing them in the workspace "C:\ti\PDK_OM~1\packages\OMAPL138\MyexampleProjects"
File Not Found
*****************************************************************************
Detecting Example Projects in PDK and importing them in the workspace "C:\ti\PDK_OM~1\packages\OMAPL138\MyexampleProjects"
Detected Example Project: cache_exampleProject
The device is not ready.
Detected Example Project: gpio_exampleProject
The device is not ready.
Detected Example Project: i2c_exampleProject
The device is not ready.
Detected Example Project: idma_exampleProject
The device is not ready.
Detected Example Project: intc_exampleProject
The device is not ready.
Detected Example Project: mddr_exampleProject
The device is not ready.
Detected Example Project: pllc_exampleProject
The device is not ready.
Detected Example Project: spi_exampleProject
The device is not ready.
Detected Example Project: timer_exampleProject
The device is not ready.
Detected Example Project: uart_exampleProject
The device is not ready.
Detected Example Project: MCASP_AudioExampleProject
The device is not ready.
Detected Example Project: MCBSP_DigLpbkExampleProject
The device is not ready.
Detected Example Project: MCBSP_MasterExampleProject
The device is not ready.
Detected Example Project: MCBSP_SlaveExampleProject
The device is not ready.
PS C:\ti\pdk_OMAPL138_1_01_00_02\packages>