Tool/software: Code Composer Studio
Hello,
I'm working on OMAP-L138 with CCS V5.5. Since the OMAP has ARM and DSP cores, I'm wondering is it possible to create one CCS project which includes the application code for both the ARM and DSP cores?
If it is possible, will the CCS create single binary file? Or there are two .out files and I need to combine those two like having two projects.
Best Regards,
Albert