Other Parts Discussed in Thread: OMAP-L138
Tool/software: Linux
Hi,
I'm setting environment for embedded linux application development with OMAP-L138 LCDK and got a problem while configuring tftp. My host is running with Windows 7, and building the uboot and kernel through Ubuntu 12.04 on VMware. The "UART-USB" of the LCDK is connect to the PC through USB cable, and the PHY of the LCDK is connected to the PC through a Ethernet-USB adapter.
After loading the uboot to the LCDK, I got something confusing:
The LCDK is given a static IP address 192.168.226.224, and the Ethernet-USB adapter is given as 192.168.226.225.
When we ping the PC from the LCDK through uboot, it works fine:
But when I try to ping the LCDK from the host (the VM is turnned off), it failed:
Regards,
Albert