Other Parts Discussed in Thread: OMAP-L132, FLASHTOOL
Tool/software: Linux
Currently I can flash the bootloader (an AIS image with U-Boot) to the NAND flash on my OMAP-L138 board using the utility "sfh_OMAP-L138.exe".
This works fine, but with disadvantages:
- I have to set a DIP switch for UART boot mode.
- This tool is a Windows prorgam.
Is there a method to update the bootloader in NAND flash (patition 1; device /dev/mtd1) directly from linux?
I've already tried with "mtd-utils"
flash_erase /dev/mtd1 0 0
nandwrite -p /dev/mtd1 <ais file>
but after that the board doesn't start after switching power off and on.