Tool/software: Linux
Hello,
I have a hardware that runs on AM1808 with Linux installed as os. For the development, I use QT creator to build an GUI based application that uses the qt 4.7.4 compiler along with ARM toolchain to build an app and installed it on this processor. The processor runs on ARM Linux Kernel 2.6.37 that uses toolchain arm2012.03 with gcc version 4.6.3
Now, I need to update the compiler version of qt that is qt 5.7 or above with the ssame toolchain. Here is the download link from where I get this...
I successfully download it and now need to configure it according to my current toolchain. For that, I update qmake.cong as below,
# # qmake configuration for building with arm-linux-gnueabi-g++ # MAKEFILE_GENERATOR = UNIX CONFIG += incremental QMAKE_INCREMENTAL_STYLE = sublib include(../common/linux.conf) include(../common/gcc-base-unix.conf) include(../common/g++-unix.conf) // modifications to g++.conf //QMAKE_CC = arm-linux-gnueabi-gcc //QMAKE_CXX = arm-linux-gnueabi-g++ //QMAKE_LINK = arm-linux-gnueabi-g++ //QMAKE_LINK_SHLIB = arm-linux-gnueabi-g++ // modifications to linux.conf //QMAKE_AR = arm-linux-gnueabi-ar cqs //QMAKE_OBJCOPY = arm-linux-gnueabi-objcopy //QMAKE_NM = arm-linux-gnueabi-nm -P //QMAKE_STRIP = arm-linux-gnueabi-strip QMAKE_CC = arm-none-linux-gnueabi-gcc QMAKE_CXX = arm-none-linux-gnueabi-g++ QMAKE_LINK = arm-none-linux-gnueabi-g++ QMAKE_LINK_SHLIB = arm-none-linux-gnueabi-g++ QMAKE_AR = arm-none-linux-gnueabi-ar cqs QMAKE_OBJCOPY = arm-none-linux-gnueabi-objcopy QMAKE_STRIP = arm-none-linux-gnueabi-strip load(qt_config)
To compile this version i use
./configure -opensource -confirm-license -prefix /usr/local/Qt5 -no-pch -xplatform linux-arm-gnueabi-g++
This is according to our current toolchain and available gcc version. The same like command I used during my old qt installation.
but we found the following error,
System architecture: 'arm' Host architecture: 'i386' arm-none-linux-gnueabi-g++ -c -fvisibility=hidden fvisibility.c Symbol visibility control enabled.
cc1plus: error: unrecognized command line option '-fuse-ld=gold' arm-none-linux-gnueabi-g++ -o libtest.so -shared -Wl,-Bsymbolic-functions -fPIC bsymbolic_functions.c bsymbolic_functions.c:2:2: error: #error "Symbolic function binding on this architecture may be broken, disabling it (see QTBUG-36129)."
Symbolic function binding disabled. checking for C++14...
arm-none-linux-gnueabi-g++ -c -pipe -O2 -std=gnu++1y -Wall -W -fPIC -I. -I../../../mkspecs/linux-arm-gnueabi-g++ -o c++14.o c++14.cpp
cc1plus: error: unrecognized command line option '-std=gnu++1y' make: *** [c++14.o] Error 1
C++14 disabled.
checking for default C++ standard edition... arm-none-linux-gnueabi-g++ -pipe -O2 -Wall -W -fPIC -I. -I../../../mkspecs/linux-arm-gnueabi-g++ -o c++default.ii -E c++default.cpp
default C++ standard edition enabled.
checking for 64-bit std::atomic... arm-none-linux-gnueabi-g++ -c -pipe -O2 -std=gnu++11 -Wall -W -fPIC -I. -I../../../mkspecs/linux-arm-gnueabi-g++ -o atomic64.o atomic64.cpp
cc1plus: error: unrecognized command line option '-std=gnu++11'
make: *** [atomic64.o] Error 1
64-bit std::atomic disabled.
checking for 64-bit std::atomic in -latomic... arm-none-linux-gnueabi-g++ -c -pipe -O2 -std=gnu++11 -Wall -W -fPIC -I. -I../../../mkspecs/linux-arm-gnueabi-g++ -o atomic64.o atomic64.cpp
cc1plus: error: unrecognized command line option '-std=gnu++11'
make: *** [atomic64.o] Error 1
64-bit std::atomic in -latomic disabled.
checking for std::atomic for function pointers... arm-none-linux-gnueabi-g++ -c -pipe -O2 -std=gnu++11 -Wall -W -fPIC -I. -I../../../mkspecs/linux-arm-gnueabi-g++ -o atomicfptr.o atomicfptr.cpp cc1plus: error: unrecognized command line option '-std=gnu++11'
make: *** [atomicfptr.o] Error 1
std::atomic for function pointers disabled.
ERROR: detected a std::atomic implementation that fails for function pointers.
Please apply the patch corresponding to your Standard Library vendor, found in /opt/qt-everywhere-opensource-src-5.7.1/qtbase/config.tests/common/atomicfptr
So, this is what I found. Can anyone suggest me a way to resolve this issue?