Other Parts Discussed in Thread: SYSBIOS, OMAPL138
Porting my code base from CCS5 to CCS8 (and using the newer libraries) I am getting lots of strange Linker warnings (like 100s) and then one unresolved symbol.
<These are examples of the Linker warnings, there are 100s of them> Note: It looks like that now all of the stuff that used to be in Utils is now in IPC. I could not see what in the CFG file forced the generation of the Utils?
------------------------------------------------------------
warning #10252-D: Symbol "EDMA3_RM_Ioctl" (pulled from "C:\ti\edma3_lld_2_12_05_30C\packages\ti\sdo\edma3\rm\lib\omapl138-evm\674\debug\edma3_lld_rm.ae674<edma3resmgr.oe674>") defined in 2 places:
C:\ti\edma3_lld_2_12_05_30C\packages\ti\sdo\edma3\rm\lib\omapl138-evm\674\debug\edma3_lld_rm.ae674<edma3resmgr.oe674>
C:\ti\edma3_lld_2_12_05_30C\packages\ti\sdo\edma3\rm\lib\omapl138-evm\674\debug\edma3_lld_rm.ae674<edma3resmgr.oe674>
...
warning #10252-D: Symbol "MultiProc_getBaseIdOfCluster" (pulled from "C:\Users\bh44962\workspace_v8\DSP_Main\src\ipc\ipc.ae674<Ipc.obj>") defined
in 2 places:
C:\Users\bh44962\workspace_v8\DSP_Main\src\ipc\ipc.ae674<Ipc.obj>
C:\Users\bh44962\workspace_v8\DSP_Main\src\utils\utils.ae674<UTILS.obj>
...
warning #10252-D: Symbol "__c6xabi_get_tp" (pulled from "C:\Users\bh44962\workspace_v8\DSP_Main\src\sysbios\sysbios.ae674<ti_tls_get_tp.obj>") defined in 2 places:
C:\Users\bh44962\workspace_v8\DSP_Main\src\sysbios\sysbios.ae674<ti_tls_get_tp.obj>
C:\ti\ccsv8\tools\compiler\ti-cgt-c6000_8.2.3\lib\rts6740_elf.lib<tls_get_tp.obj>
...
warning #10252-D: Symbol "_c_int00" (pulled from "C:\ti\bios_6_52_00_12\packages\ti\targets\rts6000\lib\boot.ae674<boot.oe674>") defined in 2 places:
C:\ti\bios_6_52_00_12\packages\ti\targets\rts6000\lib\boot.ae674<boot.oe674>
C:\ti\ccsv8\tools\compiler\ti-cgt-c6000_8.2.3\lib\rts6740_elf.lib<boot.obj>
------------------------------------------------------------
This is the one undefined symbol
------------------------------------------------------------
undefined first referenced
symbol in file
--------- ----------------
_mfence C:\Users\bh44962\workspace_v8\DSP_Main\src\ipc\ipc.ae674<Ipc.obj>
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "DSP_Main.out" not built
------------------------------------------------------------
Versions:
CCS 8.0.0.00016
Compliler: TI V8.2.3
XDCtools: 3.50.5.12_core
EDMA3: 2.12.5
IPC: 3.47.1.00
SYS/BIOS: 6.52.0.12