Other Parts Discussed in Thread: OMAP-L138, AM5728
Tool/software: Linux
software : processor-sdk-04.01.00.06;
Hardware:omap-l138 ; custom board;
Hi,
I want to use nand ubifs as rootfs, and the MTD driver was built in linux kernel, but can't mount the ubifs when booting, and MTD was not loaded at that time.
There's an error printed by kernal when booting:
UBI error: cannot open mtd rootfs, error -2console [netcon0] enabled
uboot cmdline:
nandboot=setenv bootargs console=ttyS1,115200n8 rootwait=1 rw ubi.mtd=1,2048 rootfstype=ubifs root=ubi0:rootfs
How to load MTD before the ubifs is loaded?
Other Info:
dmesg(with emmc boot, you can see mtd was loaded at filesystem-stage after kernel-stage):
OF: fdt:Machine model: DA850/AM1808/OMAP-L138 EVM Reserved memory: created CMA memory pool at 0xc3000000, size 16 MiB OF: reserved mem: initialized node dsp_cma@c3000000, compatible id shared-dma-pool cma: Reserved 16 MiB at 0xc6c00000 Memory policy: Data cache writethrough DaVinci da850/omap-l138/am18x variant 0x1 On node 0 totalpages: 32768 free_area_init_node: node 0, pgdat c06dbc50, node_mem_map c7ec9000 DMA zone: 288 pages used for memmap DMA zone: 0 pages reserved DMA zone: 32768 pages, LIFO batch:7 pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768 pcpu-alloc: [0] 0 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32480 Kernel command line: console=ttyS1,115200n8 root=/dev/mmcblk0p1 rw rootfstype=ext4 rootwait PID hash table entries: 512 (order: -1, 2048 bytes) Dentry cache hash table entries: 16384 (order: 4, 65536 bytes) Inode-cache hash table entries: 8192 (order: 3, 32768 bytes) Memory: 89688K/131072K available (4915K kernel code, 317K rwdata, 1524K rodata, 232K init, 165K bss, 8616K reserved, 32768K cma-reserved) Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xffc00000 - 0xfff00000 (3072 kB) vmalloc : 0xc8800000 - 0xff800000 ( 880 MB) lowmem : 0xc0000000 - 0xc8000000 ( 128 MB) modules : 0xbf000000 - 0xc0000000 ( 16 MB) .text : 0xc0008000 - 0xc04d5060 (4917 kB) .init : 0xc0654000 - 0xc068e000 ( 232 kB) .data : 0xc068e000 - 0xc06dd570 ( 318 kB) .bss : 0xc06dd570 - 0xc0706d68 ( 166 kB) SLUB: HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 Preemptible hierarchical RCU implementation. Build-time adjustment of leaf fanout to 32. NR_IRQS:245 clocksource: timer0_1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns Console: colour dummy device 80x30 Calibrating delay loop... 148.88 BogoMIPS (lpj=744448) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) CPU: Testing write buffer coherency: ok Setting up static identity map for 0xc0008400 - 0xc0008458 devtmpfs: initialized VFP support v0.3: not present clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns futex hash table entries: 256 (order: -1, 3072 bytes) pinctrl core: initialized pinctrl subsystem NET: Registered protocol family 16 DMA: preallocated 256 KiB pool for atomic coherent allocations cpuidle: using governor ladder cpuidle: using governor menu gpio gpiochip0: (Davinci): added GPIO chardev (254:0) gpiochip_setup_dev: registered GPIOs 0 to 143 on device: gpiochip0 (Davinci) mux: initialized RTC_ALARM mux: Setting register RTC_ALARM mux: PINMUX0 (0x00000000) = 0x00480008 -> 0x20480008 No ATAGs? edma 1c00000.edma: memcpy is disabled edma 1c00000.edma: TI EDMA DMA engine driver edma 1e30000.edma: memcpy is disabled edma 1e30000.edma: TI EDMA DMA engine driver of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator0[0]' i2c_davinci i2c_davinci.1: could not find pctldev for node /soc@1c00000/pinmux@14120/pinmux_i2c0_pins, deferring probe clocksource: Switched to clocksource timer0_1 NET: Registered protocol family 2 TCP established hash table entries: 1024 (order: 0, 4096 bytes) TCP bind hash table entries: 1024 (order: 0, 4096 bytes) TCP: Hash tables configured (established 1024 bind 1024) UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. workingset: timestamp_bits=14 max_order=15 bucket_order=1 Block layer SCSI generic (bsg) driver version 0.4 loaded (major 250) io scheduler noop registered (default) pinctrl-single 1c14120.pinmux: 160 pins at pa fec14120 size 80 Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25, base_baud = 9375000) is a TI DA8xx/66AK2x serial8250.1: ttyS1 at MMIO 0x1d0c000 (irq = 53, base_baud = 8250000) is a TI DA8xx/66AK2x console [ttyS1] enabled serial8250.2: ttyS2 at MMIO 0x1d0d000 (irq = 61, base_baud = 8250000) is a TI DA8xx/66AK2x brd: module loaded libphy: Fixed MDIO Bus: probed davinci_mdio davinci_mdio.0: davinci mdio revision 1.5 davinci_mdio davinci_mdio.0: detected phy mask fffffffe libphy: davinci_mdio.0: probed davinci_mdio davinci_mdio.0: phy[0]: device davinci_mdio.0:00, driver SMSC LAN8710/LAN8720 i2c /dev entries driver davinci_mmc da830-mmc.0: GPIO lookup for consumer cd davinci_mmc da830-mmc.0: using device tree for GPIO lookup of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/soc@1c00000/mmc@40000[0]' of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/soc@1c00000/mmc@40000[0]' davinci_mmc da830-mmc.0: using lookup tables for GPIO lookup davinci_mmc da830-mmc.0: lookup for GPIO cd failed davinci_mmc da830-mmc.0: GPIO lookup for consumer wp davinci_mmc da830-mmc.0: using device tree for GPIO lookup of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/soc@1c00000/mmc@40000[0]' of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/soc@1c00000/mmc@40000[0]' davinci_mmc da830-mmc.0: using lookup tables for GPIO lookup davinci_mmc da830-mmc.0: lookup for GPIO wp failed davinci_mmc da830-mmc.0: Using DMA, 4-bit mode NET: Registered protocol family 10 sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver NET: Registered protocol family 17 0-0020 supply vcc not found, using dummy regulator pca953x 0-0020: failed reading register pca953x: probe of 0-0020 failed with error -121 console [netcon0] enabled netconsole: network logging started davinci_emac davinci_emac.1: incompatible machine/device type for reading mac address davinci_emac davinci_emac.1: using random MAC addr: aa:b3:41:7b:e1:22 hctosys: unable to open rtc device (rtc0) vbat: disabling Waiting for root device /dev/mmcblk0p1... mmc0: new high speed MMC card at address 0001 mmcblk0: mmc0:0001 MMC16G 14.6 GiB mmcblk0boot0: mmc0:0001 MMC16G partition 1 16.0 MiB mmcblk0boot1: mmc0:0001 MMC16G partition 2 16.0 MiB mmcblk0: p1 random: fast init done EXT4-fs (mmcblk0p1): recovery complete EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null) VFS: Mounted root (ext4 filesystem) on device 179:1. devtmpfs: mounted Freeing unused kernel memory: 232K (c0654000 - c068e000) This architecture does not have kernel memory protection. systemd[1]: System time before build time, advancing clock. systemd[1]: systemd 230 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN) systemd[1]: Detected architecture arm. systemd[1]: Set hostname to <omapl138-lcdk>. systemd[1]: Listening on Journal Socket (/dev/log). systemd[1]: Listening on udev Kernel Socket. systemd[1]: Listening on /dev/initctl Compatibility Named Pipe. systemd[1]: Listening on Network Service Netlink Socket. systemd[1]: Created slice System Slice. systemd[1]: Listening on udev Control Socket. systemd[1]: Reached target Swap. EXT4-fs (mmcblk0p1): re-mounted. Opts: (null) cryptodev: loading out-of-tree module taints kernel. cryptodev: driver 1.8 loaded. systemd-journald[74]: Received request to flush runtime journal from PID 1 davinci-rproc davinci-rproc.0: assigned reserved memory node dsp_cma@c3000000 remoteproc remoteproc0: dsp is available remoteproc remoteproc0: powering up dsp remoteproc remoteproc0: Booting fw image rproc-dsp-fw, size 4536272 rtc rtc0: 1c23000.rtc: dev (253:0) omap_rtc 1c23000.rtc: rtc core: registered 1c23000.rtc as rtc0 remoteproc remoteproc0: registered virtio0 (type 7) remoteproc remoteproc0: remote processor dsp is now up SCSI subsystem initialized davinci-wdt davinci-wdt: heartbeat 60 sec libata version 3.00 loaded. ahci_da850 ahci_da850: forcing PORTS_IMPL to 0x1 ahci_da850 ahci_da850: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode ahci_da850 ahci_da850: flags: ncq sntf pm led clo only pmp pio slum part ccc usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver scsi host0: ahci_da850 ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67 ohci-da8xx: DA8XX ohci-da8xx ohci-da8xx: USB Host Controller ohci-da8xx ohci-da8xx: new USB bus registered, assigned bus number 1 ohci-da8xx ohci-da8xx: irq 59, io mem 0x01e25000 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected usb_phy_generic.0.auto supply vcc not found, using dummy regulator nand: device found, Manufacturer ID: 0xec, Chip ID: 0xdc nand: Samsung NAND 512MiB 3,3V 8-bit nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64 Bad block table found at page 262080, version 0x01 Bad block table found at page 262016, version 0x01 nand_read_bbt: bad block at 0x00000f4e0000 nand_read_bbt: bad block at 0x000013960000 2 ofpart partitions found on MTD device 64000000.nand Creating 2 MTD partitions on "64000000.nand": 0x000000000000-0x0000000a0000 : "u-boot" 0x0000000a0000-0x000020000000 : "fs" ata1: SATA link down (SStatus 0 SControl 300) davinci_nand 64000000.nand: controller rev. 2.5 davinci_mdio davinci_mdio.0: resetting idled controller SMSC LAN8710/LAN8720 davinci_mdio.0:00: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=davinci_mdio.0:00, irq=-1) IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready davinci_emac davinci_emac.1 eth0: Link is Up - 100Mbps/Full - flow control rx/tx IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready random: crng init done virtio_rpmsg_bus virtio0: rpmsg host is online virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x3d musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected mtd: exports duplicate symbol mtd_concat_create (owned by kernel) mtd: exports duplicate symbol mtd_concat_create (owned by kernel) NET: Registered protocol family 43
Thank you,
Andi