• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » OMAP™ Processors » OMAP-L13x, AM1x and C674x Processors Forum » All Tags » AUDIO
Share
OMAP™ Processors
  • Forums
  • Announcements

Browse by Tags

OMAP™ Processors

Welcome to the OMAP™ Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
AUDIO
  • AM1808
  • C6747
  • c6748
  • C674x
  • C6Run
  • Codec Engine
  • DSP/BIOS
  • EDMA
  • L137
  • L-138
  • Linux
  • McASP
  • McBSP
  • OMAP
  • omap l137
  • OMAP L-137
  • omap l138
  • OMAP L-138
  • OMAPL137
  • OMAPL-137
  • OMAP-L137
  • OMAPl138
  • OMAP-L138
  • OMAPL13x
  • SPI
Related Posts
  • Forum Post: Re: USB Host controller

    Juan Gonzales Juan Gonzales
    My initial thought is that our SDK drivers (which I assume you are using) are written for the Mistral OMAP35x EVM, which only supports stereo 2-channel output. I do not believe the hardware (and probably Linux drivers) can handle 6-channels.
    on Sep 25, 2008
  • Forum Post: McBSP and 192KHz/24bit codec

    Christos Nikolaou12204 Christos Nikolaou12204
    Hi, I have a C2 Beagleboard and I've built a prototype codec daughter board that is I2C controlled and has dedicated 12.288MHz circuitry. The codec is 192KHz/24bit and needs 2 full duplex stereo I2S ports (McBSP) to be connected. I'm trying to identify what is the easiest way to create...
    on May 26, 2009
  • Forum Post: C6747 McASP driver in master mode

    Sergio Martins Sergio Martins
    Hello I've been having some problems in getting the McASP driver running in master mode and both the examples that come with the pspdrivers_01_30_00_06 are in slave mode. The problem i'm having is the fact that i can control the clock generation, but the framesync generation is not working...
    on Feb 12, 2010
  • Forum Post: Re: Audio Sample Project Buffer problem

    Fikret Alim Fikret Alim
    Hi, again Can this problem be related with the usage of DMA? Is the DMA used or not used in the default configurations of audioSample.pjt given inside pspdrivers. I am doubtful about this issue, because inside the mcasp channel parameter settings inside the code, "IsDmaDriven" is set as...
    on Jun 3, 2010
  • Forum Post: changing in/output-sources and sample rate of the psp audio sample

    Rico Schulze Rico Schulze
    Hello, i am currently running the audio sample from the pspdriver in the 01_20_00 -version and it works quiet well. But i would be interested to use also the MIC_IN and HP_OUT Connections of the board, and to change the Sample-Rate (simply changing the sampling rate in the audioSample_io.c-File...
    on Jul 15, 2010
  • Forum Post: sound access using tasks of DSP/BIOS

    Rico Schulze Rico Schulze
    Hello as someone who is new to TI-products i learned programming the DSP-Side of the OMAP L137/TMS320C6747 using the offered example codes with CodeComposerStudio 3.3 But now that i am trying to "mix" these examples in order to develope my own program, i am getting in trouble. I would...
    on Jul 13, 2010
  • Forum Post: Help for Multichannel Audio Board for DA830 EVM / OMAP-L137

    PENGFEI JIANG PENGFEI JIANG
    Hi! We are using the OMAP_L137 for microphone array signal processing ,now we only have the OMAP_L137 EVM,so we want to have multiplechannel audio board . The 702222 is a Multichannel Audio Board for DA830 EVM / OMAP-L137 Starter Kit, before buying it, I want to check that if it can be connected...
    on Jul 19, 2010
  • Forum Post: Questions about OMAPL137 EVM for microphone array signal processing

    Bo Li53615 Bo Li53615
    I'm really new to OMAPL- series and now I will develop a microphone array speech signal processing (enhancement) platform on OMAP-L137 EVM (I only got this board). So, I got one question: can anybody give me any advice that which audio board should I choose directly be used for my project? I have...
    on Jul 19, 2010
  • Forum Post: Re: moving audio-sample into another project / Linking trouble

    Rico Schulze Rico Schulze
    i tried to rebuild the sample project, using the source-code of the Audio-sample of the PSP.I included the source-code-files into a newly created,empty project and created the DSP/BIOS-Configuration-File on my own. I even copied the compiler and Linker parameters. But even this resulting project, which...
    on Jul 26, 2010
  • Forum Post: program crashes performing FFT / IFFT

    Rico Schulze Rico Schulze
    Hello, I have a project, running a network and an audio task. The Audio task echos back the original sound on the left-ear-chanel, and on the right channel it performs a FFT and afterwards an IFFT and echos back the result of it, to compare the result to it's original. I am using the FFT and...
    on Aug 9, 2010
  • Forum Post: In omap-L137 audio example,sound is only present in the left of my headphone

    xiang lee xiang lee
    Hi. I’ m a new user of OMAP-L137 EVM rev. D and I have a problems to solve.I have used the audio example (its probject name is audioSample.pjt) in BIOSPSP_01_30_01.It can run but the sound is present in the left of my headphone. I don't know why,Can anyone tell me why?I am anxious about...
    on Jan 11, 2011
  • Forum Post: Re: Problem with 32-bit audio on OMAP L137 EVM

    Rico Schulze Rico Schulze
    Normal 0 21 false false false MicrosoftInternetExplorer4 Drew, Thanks for your suggestion. The McASP data is fine in the digital loopback mode. Probably this is an AIC310 configuration issue. Again, as long as the received stream...
    on May 3, 2011
  • Forum Post: Problem with 32-bit audio on OMAP L137 EVM

    Rico Schulze Rico Schulze
    Hello, I am using the audio example of the PSP version 1.30 with the OMAP L137 EVM board. The code was modified like described in post http://e2e.ti.com/support/embedded/f/355/p/42576/165541.aspx#165541 to use the 32-bit mode of the codec in a non-interleaved stream. The data of the stream seems to...
    on Apr 28, 2011
  • Forum Post: Re: Record sound on SATA with OMAP L138 via LINE IN

    Hubert Launay Hubert Launay
    Right, I 'm actually trying to develop an application on the ARM to record data into SATA . But not only . The record data are audio data ( files.wav ) which comes from the input connector across the TLV320AIC3106 audio codec . So I want to encode the audio data on the DSP salve power on ARM ...
    on May 16, 2011
  • Forum Post: Re: Omap L138 -Adaptive audio filter

    pop iulia pop iulia
    Thanks for the reply , Drew. Now I have a new question.I used ...\Sols\lab6 - PRD\Project to separate L/R audio channel but when I run the project I hear to the headset (which is connected to LINE OUT of OMAP L138 board) some noise , even if I do not send anything on LINE IN .If I send a signal on...
    on May 19, 2011
  • Forum Post: Re: Omap L138 -Adaptive audio filter

    pop iulia pop iulia
    Yes , I am using the BIOS Workshop Training Labs and I have the board connected to a computer via USB.I am using the default boot mode , SPI1 Flash and if I removing the USB connection when the program is running , then the program no longer running . If I change the source code from ...\Sols\lab6...
    on May 23, 2011
  • Forum Post: DSP starter kit with 4 simultaneously sampling audio inputs.

    Jan Minck Jan Minck
    Hi, I have to start on an DSP application which requires 4 audio inputs sampling at ~44kHz simultaneously. (this because the phase shift between the signals is important) Because I have to perform FFT and FFT-1 on all the 4 signals I would need a DSP with a bit of grunt but with low power...
    on Jul 1, 2011
  • Forum Post: Help needed regarding Audio using SDMA and McBSP

    Munam Hafeez Munam Hafeez
    Hello All, I am working on the BeagleBoard for playing Audio. I am writing my own driver for it. I use SDMA to transfer my audio data to McBSP2 using software triggering. The data is sent in 1k chunks because of the FIFO size limitation. I have registered interrupt on end-of-block-transfer for SDMA....
    on Aug 3, 2009
  • Forum Post: AM1808 EVM

    Viral Sachde Viral Sachde
    Hi, I wish to use AM1808 in my design but wish to try it before on EVM. I found that Spectrum Digital EVM[1] is not available for retail sale and only LogicPD EVM[2] is available. I want to know which all pins are available on header so I can make daughter card and experiment it. Specially, I'm...
    on Dec 4, 2011
  • Forum Post: Dropping audio samples with EDMA and McASP

    Brian Flinn Brian Flinn
    (Please visit the site to view this file) Attached are 4 files of for a test case to try to make edma with the McASP work on our hardware, and Logic PD zoom OMAP_L138 EVM This is a modification of the source found at http://software-dl.ti.com/dsps/dsps_public_sw/c6000/web/c6747_audio_edma_app...
    on Dec 4, 2011
  • Forum Post: Adding second xmt D/A to McASP / edma OMAP-L138

    Brian Flinn Brian Flinn
    Note: This is a modification of the source found at http://software-dl.ti.com/dsps/dsps_public_sw/c6000/web/c6747_audio_edma_app/latest/index_FDS.html c6747_audio_edma_v4.zip modified for use with OMAP_L138 ect.. on our hardware. Attached are 3 files (Please visit the site to view this file) for...
    on Dec 18, 2011
  • Forum Post: Re: Stereo audio with evmomapl137

    Joe Coombs Joe Coombs
    Guillaume, Does the data appear different during the processing phase of your application? You may also want to try something drastic (i.e. zero out the left channel) to see if you can force any difference between the channels. Also, what did you use as the starting point for your application development...
    on Jan 19, 2012
  • Forum Post: Re: OMAP L137 Output Voltage

    Joe Coombs Joe Coombs
    Tobias, The values in your data buffers should "max out" at the extreme levels input/output by the audio codec. The codec can also be configured to output or accept different data formats. For example, in 32-bit unsigned integer mode, a value of 0 corresponds to the minimum analog level...
    on Jan 25, 2012
  • Forum Post: Re: voip in omapl137/tms 320c6747 - examples please

    Joe Coombs Joe Coombs
    tharangini, I'm not aware of any example applications that combine NDK usage with audio passthru on C6747/OMAP-L137, but there are several examples demonstrating audio passthu with ping pong buffering. One simple example that uses BSL-style code to control the McASP peripheral can be downloaded...
    on Feb 2, 2012
  • Forum Post: EDMA3 McASP CSL problem on OMAP L138

    Terence HUERTAS Terence HUERTAS
    Hi, I'm trying to setup EDMA3 with CSL for the DSP side of the OMAP L138 in order to gather samples into buffers from the onboard TLV320AIC3106 of my experimenter kit. Two DSP examples from http://processors.wiki.ti.com/index.php/QuickStartOMAPL1x_rCSL were used for this EDMA 3 project as a...
    on Jul 6, 2011
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use