• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » OMAP™ Processors » OMAP-L13x, AM1x and C674x Processors Forum » All Tags » OMAP L-138
Share
OMAP™ Processors
  • Forums
  • Announcements

Browse by Tags

OMAP™ Processors

Welcome to the OMAP™ Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
OMAP L-138
  • AM1808
  • boot
  • c6748
  • C674x
  • DSP
  • DSP/BIOS
  • DSP/BIOS Link
  • dsplink
  • EDMA
  • l138
  • L-138
  • Linux
  • McASP
  • OMAP
  • omap l137
  • OMAP L-137
  • omap l138
  • OMAP_L138
  • omap3530
  • OMAPL137
  • OMAP-L137
  • OMAPl138
  • OMAP-L138
  • omapl138 boot
  • omap-l138 L138
Related Posts
  • Forum Post: Is it possible OMAP L-138's sATA I/F connect to Camera which has sATA I/F?

    rs3301 rs3301
    OMAP L-138 has sATA I/F as you know. Is it possible can connect with Camera device which has sATA I/F like this below URL http://www.artray.us/3.html Thank you for advance.
    on Jan 27, 2011
  • Forum Post: OMAPL138 USB 1.1 Host port in U-Boot?

    Henrik Abrahamsson Henrik Abrahamsson
    Hi, I have an OMAPL138 based custom board and would like to use the USB 1.1 Host port in U-Boot. Is there any support for this in the PSP-package or do I have to write my own driver? I can only find support for the USB 2.0 OTG port. I really thought it was a common thing to use the USB host port in...
    on Feb 7, 2011
  • Forum Post: Accessing the UPP (Parallel port) from the DSP side of the L138

    David Nizel David Nizel
    (Please direct to Tim H. Customer request from Ft. Lauderdale. Thank you. -DN) Could help me find sample code that accesses the UPP (Parallel port) from the DSP side of the L138? Ideally if we can find code that uses or can be converted to take advantage of the C6Run or C6APP arm-dsp software interface...
    on Feb 18, 2011
  • Forum Post: RTC-controlled deep sleep on OMAPL138

    nchukeg nchukeg
    Hello, On OMAPL138 after configuring internal RTC and going into deep-sleep, is it possible to turn off the power to the processor (except for the RTC power pins) and still have RTC generate an interrupt? The idea is to have an external hardware logic that shuts off the power to the OMAPL138...
    on Feb 23, 2011
  • Forum Post: Using DSPLink on OMAPL138 where L1 and most of L2 are protected from external access

    nchukeg nchukeg
    Hello, We are using OMAPL138. ARM core is used by the customer and DSP core has our proprietary code. L1 is set up as cache and L1/L2 are fully protected from external access EXCEPT for 1 or 2 data pages. We would like to be able to use DSPLink to communicate between the two processors. 1...
    on Feb 1, 2011
  • Forum Post: OMAPL138 PLL set-up

    nchukeg nchukeg
    Hello, We are using OMAPL138. Is it OK for device speed range 4 (456 MHz) to configure the output of PLL1 (after the POSTDIV) to be above 456 MHz as long as PLLDIV1 and PLLDIV2 for PLL1 will be configured to reduce the frequency to within 300 MHz and 152 MHz? Thanks Oleg
    on Feb 28, 2011
  • Forum Post: Sharing 64-bit timer on OMAPL138 for Linux and BIOS clocks

    nchukeg nchukeg
    Hello, On OMAPL138, is it possible to configure 64-bit Timer 0 as two 32-bit unchained timers and use them as OS clocks for Linux running on the ARM and BIOS running on the DSP? Or will BIOS can interfere with the operation of the other timer during the configuration step for example? And more...
    on Mar 1, 2011
  • Forum Post: MatLab OMAPL138 support?

    David Nizel David Nizel
    Question: Is MatLab support for OMAPL138 anticipated, and if so, when and to what extent? It would be desirable for Matlab to generate code for OMAPL138. Thank you. -DN
    on Mar 3, 2011
  • Forum Post: AINTC nested interrupts code examples

    Fredrik M���ller Fredrik M���ller
    Are there any free code available which shows how to configure the ARM interrupt controller (AINTC) on the OMAP-L138 for supporting nested interrupts? The "Applications Processor System Reference Guide" (SPRUGM7D, April 2010) documents how to perform nesting in chapter 12.3.7. The 11-step...
    on Mar 14, 2011
  • Forum Post: OMAP-L138 Schematic Review Checklist and Datasheet discrepancy

    TommyG TommyG
    I am going through the Schematic Review Checklist for the OMAP-L138 located in Wiki page here: http://processors.wiki.ti.com/index.php/OMAP-L13x_/_C674x_/_AM1x_Schematic_Review_Checklist#Decoupling_Capacitors . In the section on decoupling capactitors the checklist directs to go to datasheet section...
    on Mar 16, 2011
  • Forum Post: missing spi.ini file in OMAP-L138_FlashAndBootUtils_2_11

    Anthony Glaser Anthony Glaser
    According to the document GSG: Da8x/OMAP-L1/AM1x DVEM Additional Procedures on page 9 there is supposed to be a file called OMAP-L138_EVM_spi.ini file in the FlashAndBootUtils_2_11.tar.gz. I've downloaded and untarred the FlashAndBootUtils_2_11.tar.gz file and it doesn't seem to be there....
    on Mar 18, 2011
  • Forum Post: Re: Power-on and Warm reset on OMAP-L138

    Boris Ruvinsky Boris Ruvinsky
    Hello Drew. Thank you for your answer to my question. There are some extra little details which I would like to know. Is there the requirement for TRSThigh setup to WARM_RESETlow? If TRST is latched by RESEThigh-to-low edge - there should be some requirement for setup. The TRST hold is...
    on Apr 14, 2011
  • Forum Post: OMAPL138 UPP Receiver

    Ben Campbell Ben Campbell
    (Please visit the site to view this file) Hello, Please can you help me to get a simple UPP receiver working on the OMAPL138? I am using the Avnet OMAP/Spartan6 platform. I am using dsp/bios 5.41.03.17, code gen tools 6.1.9, ccs4, pspdrivers 01.30.01. I can get the pspdriver UPP loopback example...
    on Apr 20, 2011
  • Forum Post: Re: omapl138 <> micron 256Mb DDR2 problem

    Cor Cor
    Hello Jeff, 1) I use series resistors off 22ohms on all lines 2) The revision is MT47H16M16BG-3:B 3) Yes I tried this at tCK is 8ns->125MHz which is the lowest clock for this ddr2 -3 4) Yes I started with the spreadsheet. and then afterwards I used the SPRUGJ4B user guide to understand...
    on Apr 21, 2011
  • Forum Post: EDMA Configuration - Two Channels, OMAP-L138

    Alexey Tsirlin Alexey Tsirlin
    Hi, I am trying to use two EDMA channels in parallel. One channel is driving SPI DAC and the second channel is used for copying data chunk from SDRAM (connected to EMIFA) to DSP L2 RAM, I am using some unused DMA channel for this purpose (let's say channel 0). The SPI DMA channel is configured...
    on Apr 21, 2011
  • Forum Post: Re: The limit write and read speed applying SATA2 interface of OMAP-L138 chip

    Xingwang Xu Xingwang Xu
    Hi Jeff, Thanks for your help. A filesystem is necessary for me to make it easier to read the data in the harddisk on Windows OS. Is the 21.6MB/s write performance @300MHz of OMAP-L138 the limiting performance? Is the write performance conneted to the cpu clock speed? Cause I care the write performance...
    on Apr 28, 2011
  • Forum Post: Re: omapl138 <> micron 256Mb DDR2 problem

    Cor Cor
    Hi Jeff, Due to an isolation problem in one of the layers the ddr_dqgate0 was shorted to ground. I got a strange behavior of the ddr2 by this fault. regards, Cor
    on Apr 28, 2011
  • Forum Post: OMAP-L138 Experimenter board - Flash Utility Problem

    Andres Gomez Andres Gomez
    I'm trying to erase SPI Flash on Experimenter board. On the cmd line I'm trying "sfh_OMAP-L138.exe -erase" "Waiting for SFT on the OMAP-L138..." and nothing happens. It hangs.... Any suggestions? Are there other ways to load an image into flash for the experimenter...
    on Apr 28, 2011
  • Forum Post: AISgen for OMAP-L138

    Frank Frank
    Hello, I've some questions to AISgen (Version 1.7c). We will start soon to replace the L137 with L138, where the boot concept is different, as the L138 is an ARM-boot device. On the following page http://processors.wiki.ti.com/index.php/Boot_Images_for_OMAP-L138 under "Description"...
    on Apr 21, 2011
  • Forum Post: Re: OMAPL138 Experimenter : setup.sh : Problem during Load uboot script

    Hubert Launay Hubert Launay
    I changed the bootargs like this : but it still does not work .
    on May 5, 2011
  • Forum Post: Re: OMAPL138 Experimenter : setup.sh : Problem during Load uboot script

    Hubert Launay Hubert Launay
    Indeed , it works well ... Thank you for your help . For information, here is my final configuration of U - boot:
    on May 9, 2011
  • Forum Post: XDS 510 USB PLUS driver for OMAP L138

    SHAMEEM SHAMEEM
    Hai We intent to buy a XDS 510 PLUS JTAG emulator for our development on OMAP L138 based platform. We have to make sure whether the XDS 510 USB PLUS supports OMAP L138. ie whether drivers are available for the same? Regards Shameem
    on May 12, 2011
  • Forum Post: OMAP-L138 Local reset is not done

    Frank Frank
    Hello, I'm using a LOGIC PD L138 eXperimenter board with the following versions on the ARM side of the OMAP-L138: - CCS Version 4.2.1.00004 - SYS/BIOS 6.30.03.46 On the DSP side I'm using the (slightly modified) led_dip project/image contained in the 1017292B_OMAP-L138_GEL_BSL_Files_v2...
    on May 20, 2011
  • Forum Post: OMAP-L138 EVM version compatibility

    Don Froese Don Froese
    We recently bought a second TMDSEVLM138 OMAP-138 EVM and are unable to run the code we developed on our original OMAP-138 EVM. We are using the TMS320C6748 DSP SOM on both boards. The original EVM came with rev A of the SOM and the new EVM came with rev B of the SOM. The code crashes on the new board...
    on May 31, 2011
  • Forum Post: Omap-L138 Power Spread Sheet

    Boris Ruvinsky Boris Ruvinsky
    Dear E2E: I use Omap-L138. Omap-l138 has two I2C interfaces I2C0 and I2C1. Omap-L138 Power Spreadsheet (V.B and V.C) allows enabling I2C1 only. http://processors.wiki.ti.com/index.php/OMAP-L138_Power_Consumption_Summary " I2C0 is grayed out and can't be enabled. How to enable...
    on Jun 9, 2011
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use