This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Standard template library vector class on the DSP side of the OMAP-L138 bug?

Has anyone used the standard template library vector class on the DSP side of the OMAP-L138?

I have a large memory intensive algorithm that is being adapted from a corresponding MATLAB
program and up til now have been using STL vector with success, albeit the expected performance
hit. At the moment speed is not as important as algorithmic correctness.

I have just discovered that at a certain point in my algorithm during the instantiation of
a vector object the memory that is occupied by the vector object conflicts (lies on top of) of a previously
allocated vector object. The heap does not appear to be exhausted as I have set aside approx 12 Mbyte for the
heap in the DSP-BIOS configuration and the returned address for the object appears to indicate that only about 1Mbyte has been utilized
at the time of the strange behavior.

I am using tool chain version 6.1.9 under Code Composer Studio v. 3.3

I was wondering if anyone else has experienced this in use of the vector class or if this is known behavior and there is a remedy.

-Richard