One further piece of information...this is a CUS package of OMAP 37XX which I am working with. The pin which I am MUXING for GPIO126 is "N22" Again when I change pull up/pull down on the PAD, the voltage (read with a meter) on this pad goes from .03 to 0 volts...so I am hitting the right pad.
We found the answer. VDD_X. We connected it to VDD_MMC1 so GPIO126 could work