I'm having no luck getting anything out of the rx register of the omap spi on port 4. I have scoped the data on all four signals connected to a touchscreen controller and the signals look exactly like I would expect. In fact, the chip-select, SIMO and clock lines are working fine from the omap and data is being sent back from the touchscreen controller as expected. The problem is that I can't seem to get anything but zeros out of the rx register. There doesn't seem to be a problem with my muxing (spi4 somi is set to only one pin and the mode on the pin is correct).
I'm curious if anyone else has tried to use the spi on the OMAP35xx series with success. Because right now it would seem that there's either a major issue with the mcspi driver in Linux (which as far as I can tell is correct) or there is a problem in the hardware. If someone has had it working then please let me know under what circumstance.
~Kevin
Would you post your register settings for the PAD configuration for SPI4? We can at least start there and determine if everything is in order.
The register which controls mcspi4_somi is CONTROL_PADCONF_MCBSP1_DX at 0x48002190. Just a quick thought, but you should make sure the INPUTENABLE bit is set.
Brandon
This is the dmesg output from my printk in the mcspi driver (specifically the omap2_mcspi_txrx_pio function).
[ 72.464597] (>")> omap2_mcspi_txrx_pio MCSPI_CHxCONF = 001313D4[ 72.470761] (>")> omap2_mcspi_txrx_pio CONTROL_PADCONF_MCBSP1_DX = 01010001
I know that the CHxCONF is set for rx only mode. The system sends out a byte then reads in two (as per the tsc2046 requirements). Again, the correct signals are on all four lines for the spi4 and I have verified that it is physically connected correctly by toggling GPIO and scoping the lines.
Sorry I hadn't gotten to this. Do you have any status update on your efforts to receive on the SIMO input?
We worked on it for another day or so before we just modified the touchscreen driver to bitbang the spi. I'm going to keep an eye on it because we would prefer to use the hardware but I'm pretty hopeless.
Have you seen recent activity on the beagleboard@googlegroups.com mailing list regarding MCSPI functionality?
It appears Mr. Balister has made some progress in this endeavor as it relates to the Linux kernel having its own PINMUX setup and other configuration beyond what something like u-boot is doing.I'm not sure if this is directly applicable to your efforts, but given the subject of the RX path always receiving 0s is the same, it seems plausible to be related.
Kevin,
I had the same problem and resolved it the same way you did... I spent about 3 days working on the SPI interface to my LCD controller (on a CSB740 board). Verified with scope that all pins were functioning correctly, but never saw a thing on the rcv register (all zeroes). Then spent 15 minutes implementing it with bit-banging and it worked just fine. Sure would like to know the secret (assuming its not a silicon bug in the OMAP35xx). In my case, I'm not using u-boot or linux, this is a port of MicroMonitor. Regardless, it sure would be nice to switch back to SPI mode in place of the bit-banger.
If you ever get an answer on this, I'd sure like to hear about it.
Thanks
Ed
Is the INPUTENABLE to the mcspi*_clk enabled? Although the functional clock to the McSPI interface is on inside the device and clocking the TX state machine, the mcspi*_clk pin is wrapped back inside the device to actually sample the mcspi*_somi input.
Brandon,
Hmmm... I missed your earlier point regarding this :-(.
I see that it isn't set in my code. I'll try changing this and let you know (can't do it till tonight).
Thanks, Ed
Thanks much... I made that change and that fixed it...
I had this exact same problem and struggled for days. It needs to be explaned in the data manual the clk pad needs to be configured as input.
I lost 4 days on this problem trying to program McSPI1 from the C64x+ side. I concur that TI needs to add this crucial detail to the McSPI manual!!
Hi,
Can anyone please let me know why pull down resistor is required on McSPI1_CLK line?
I have seen in beagle board, there also pull down is given.
Please let me know.
Regards,
Murugan
AFAIR the pull down on the McSPI1_CLK line on BeagleBoard is only for BeagleBoard revision detection. The pin on Beagle isn't used in SPI-mode, but in GPIO-mode (GPIO171) together with GPIO172 for board ID detection. Using the pin in SPI-mode won't require the pull down.
Best regards Søren
Søren Steen Christensen - SSC Solutions ApS - Web: www.ssc-solutions.dk
I try MIDAS v2.0 following web sitehttp://processors.wiki.ti.com/index.php/MIDAS_Ultrasound_v2.0_Demo
I think that I succeeded compile in everything except touch screen.
I try Touchscreen Setup follow web site blow.
Touchscreen Setup
MIDAS utilizes the tslib library for touchscreen support on the OMAP3530 EVM. This section will guide you through setting up tslib.
1. Install required packages on host
host $ sudo apt-get install autogen autoconf libtool
2. For cross-compiling, define environment variables in ~/.bashrc on host as:
export CC=/home/<username>/arm-2009q1/bin/arm-none-linux-gnueabi-gcc export CXX=/home/<username/arm-2009q1/bin/arm-none-linux-gnueabi-g++ export CONFIG_SITE=omap3evm.autogen
3. Download the source files for tslib from here and save it at ~
4. Untar the source
host $ cd ~host $ tar xjf tslib-1.0.tar.bz2
5. Configure tslib
host $ cd ~/tslib-1.0 host $ ./autogen.sh host $ ./configure --prefix=/home/<username>/workdir/filesys --host=arm-linux-gnu
6. Comment the line ‘AC_FUNC_MALLOC’ in ~/tslib-1.0/configure.ac
7. Comment ‘#define malloc rpl_malloc’ in ~/tslib-1.0/config.h if it exists
8. Build and install tslib
host $ make host $ make install
9. Edit ~/workdir/filesys/etc/ts.conf to use linux layer event interface by uncommenting ‘module_raw input’
10. Modify the device’s startup script to export the required touchscreen related environment variables.
Add these lines to the file ~/development/workdir/filesys/etc/profile:
export QWS_MOUSE_PROTO='Tslib:/dev/input/event1' export TSLIB_CALIBFILE='/etc/pointercal' export TSLIB_CONFFILE='/etc/ts.conf' export TSLIB_CONSOLEDEVICE='none' export TSLIB_FBDEVICE='/dev/fb0' export TSLIB_PLUGINDIR='/lib/ts' export TSLIB_TSDEVICE='/dev/input/event1'
11. Remember to run ‘ts_calibrate’ on the target the first time you start the board, to calibrate the touch screen.
I inputed command ts_calibrate and I get some message blow.
omap3evm login: root
root@omap3evm:~# ts_calibrateNo raw modules loaded.ts_config: Successroot@omap3evm:~#
root@omap3evm:~# <4>omap-dss: Could not find exact pixel clock. Requested 25188 kHz, got 25187 kHzomap-dss: Could not find exact pixel clock. Requested 25188 kHz, got 25187 kHz
I'm looking for "Could not find exacpt pixel clock" at google and e2e.ti.com.
I found a TI member as same error message. ( http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/t/94126.aspx )
But I didn't get enough answer.
So I try that as indicated.
First, I input command ls -la /dev/input.
root@omap3evm:~#
root@omap3evm:~# ls -la /dev/input/
drwxr-xr-x 2 root root 100 Jan 1 1970 .
drwxr-xr-x 10 root root 3060 Sep 11 16:17 ..
crw-r----- 1 root root 13, 64 Jan 1 1970 event0
crw-r----- 1 root root 13, 65 Jan 1 1970 event1
lrwxrwxrwx 1 root root 6 Jan 1 1970 touchscreen0 -> event1
Second, I input command cat /proc/bus/input/devices
root@omap3evm:~# cat /proc/bus/input/devices
I: Bus=0019 Vendor=0001 Product=0001 Version=0003
N: Name="omap_twl4030keypad"
P: Phys=omap_twl4030keypad/input0
S: Sysfs=/class/input/input0
U: Uniq=
H: Handlers=kbd event0
B: EV=100003
B: KEY=1680 0 70032 53840000
I: Bus=0000 Vendor=0000 Product=0000 Version=0000
N: Name="ADS784x Touchscreen"
P: Phys=spi1.0/input0
S: Sysfs=/class/input/input1
H: Handlers=event1
B: EV=b
B: KEY=400 0 0 0 0 0 0 0 0 0 0
B: ABS=1000003
3th, I input command cat /dev/input/event0 & 1 and touch screen.
root@omap3evm:~# cat /dev/input/event0
There is no response when I touched the screen.
I input command cat /dev/input/event1 & touch screen.
There is something reactions.
root@omap3evm:~# cat /dev/input/event1
}z▒JǗ~z▒J▒J~z▒J▒~z▒Jz▒J▒:z▒Jz▒J▒:
z▒J▒:z▒J▒z▒Jz▒J▒d
▒J▒dz▒J▒dPuTTYPuTTYPuTTYPuTTYPuTTYPuTTYPuTTYPuTTYPuTTz▒Jz▒J▒▒
z▒J▒▒z▒J▒z▒J]
z▒J]z▒Jz▒J>▒z▒J>▒▒ z▒J>▒z▒J>z▒J▒z▒J▒▒ z▒J▒z▒Jz▒J▒9z▒J:▒ z▒Jz▒J▒yz▒J▒yv z▒J▒yz▒J▒z▒J▒▒z▒JΚh z▒JΚz▒Jz▒J▒▒z▒J▒▒> z▒J▒z▒Jz▒J6m z▒J6z▒Jz▒Jgz▒Jz▒Jgz▒Jz▒J▒
z▒J▒
z▒J▒▒ z▒J▒▒ z▒J▒▒ z▒J▒▒ z▒J▒ z▒J▒ z▒J/▒
4th, I input command ls -la /lib/ts
root@omap3evm:~# ls -la /lib/ts/
drwxr-xr-x 2 1000 1000 4096 Apr 27 2012 .
drwxr-xr-x 6 1000 root 4096 Apr 27 2012 ..
-rwxr-xr-x 1 1000 1000 944 Apr 27 2012 arctic2.la
-rwxr-xr-x 1 1000 1000 5631 Apr 27 2012 arctic2.so
-rwxr-xr-x 1 1000 1000 938 Apr 27 2012 collie.la
-rwxr-xr-x 1 1000 1000 10498 Apr 27 2012 collie.so
-rwxr-xr-x 1 1000 1000 932 Apr 27 2012 corgi.la
-rwxr-xr-x 1 1000 1000 5597 Apr 27 2012 corgi.so
-rwxr-xr-x 1 1000 1000 950 Apr 27 2012 dejitter.la
-rwxr-xr-x 1 1000 1000 6658 Apr 27 2012 dejitter.so
-rwxr-xr-x 1 1000 1000 932 Apr 27 2012 h3600.la
-rwxr-xr-x 1 1000 1000 5625 Apr 27 2012 h3600.so
-rwxr-xr-x 1 1000 1000 932 Apr 27 2012 input.la
-rwxr-xr-x 1 1000 1000 7163 Apr 27 2012 input.so
-rwxr-xr-x 1 1000 1000 938 Apr 27 2012 linear.la
-rwxr-xr-x 1 1000 1000 8810 Apr 27 2012 linear.so
-rwxr-xr-x 1 1000 1000 974 Apr 27 2012 linear_h2200.la
-rwxr-xr-x 1 1000 1000 6368 Apr 27 2012 linear_h2200.so
-rwxr-xr-x 1 1000 1000 932 Apr 27 2012 mk712.la
-rwxr-xr-x 1 1000 1000 5629 Apr 27 2012 mk712.so
-rwxr-xr-x 1 1000 1000 938 Apr 27 2012 pthres.la
-rwxr-xr-x 1 1000 1000 6479 Apr 27 2012 pthres.so
-rwxr-xr-x 1 1000 1000 944 Apr 27 2012 ucb1x00.la
-rwxr-xr-x 1 1000 1000 5535 Apr 27 2012 ucb1x00.so
-rwxr-xr-x 1 1000 1000 950 Apr 27 2012 variance.la
-rwxr-xr-x 1 1000 1000 6545 Apr 27 2012 variance.so
5th, I input command cat /etc/ts.conf
root@omap3evm:~# cat /etc/ts.conf
# Uncomment if you wish to use the linux input layer event interface
# module_raw input
# Uncomment if you're using a Sharp Zaurus SL-5500/SL-5000d
# module_raw collie
# Uncomment if you're using a Sharp Zaurus SL-C700/C750/C760/C860
# module_raw corgi
# Uncomment if you're using a device with a UCB1200/1300/1400 TS interface
# module_raw ucb1x00
# Uncomment if you're using an HP iPaq h3600 or similar
# module_raw h3600
# Uncomment if you're using a Hitachi Webpad
# module_raw mk712
# Uncomment if you're using an IBM Arctic II
# module_raw arctic2
module pthres pmin=1
module variance delta=30
module dejitter delta=100
module linear
What is the problem?
Please tell me the solution.
Additional noted items.
root@omap3evm:~# dmesgLinux version 2.6.29-rc3-omap1 (won@ubuntu) (gcc version 4.2.3 (Sourcery G++ Lite 2008q1-126)) #6 Thu Apr 26 19:45:05 KST 2012
CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c5387f
CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
Machine: OMAP3 EVM
Memory policy: ECC disabled, Data cache writeback
On node 0 totalpages: 58112
free_area_init_node: node 0, pgdat c0440c24, node_mem_map c0465000
Normal zone: 512 pages used for memmap
Normal zone: 0 pages reserved
Normal zone: 57600 pages, LIFO batch:15
OMAP3530 ES3.1 (full speed SGX, IVA2)
SRAM: Mapped pa 0x40200000 to va 0xd7000000 size: 0x100000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 57600
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.1.100:/home/won/workdir/filesys,nolock mem=99M@0x80000000 mem=128M@0x88000000 mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
Clocking rate (Crystal/DPLL/MPU core): 26.0/332/500 MHz
IVA2 clocking rate: 360 MHz
Reprogramming SDRC
GPMC revision 5.0
IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts
Total of 96 interrupts on 1 active controller
OMAP34xx GPIO hardware version 2.5
PID hash table entries: 1024 (order: 10, 4096 bytes)
OMAP clockevent source: GPTIMER1 at 32768 Hz
Console: colour dummy device 80x30
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 99MB 128MB = 227MB total
Memory: 225664KB available (3928K code, 370K data, 156K init)
Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
net_namespace: 520 bytes
NET: Registered protocol family 16
MUX: setup AF26_34XX_GPIO0 (0xd80021e0): 0x011c -> 0x0118
MUX: setup L8_34XX_GPIO63 (0xd80020ce): 0x0118 -> 0x0004
MUX: setup AF9_34XX_GPIO22 (0xd80025ec): 0x0100 -> 0x011c
MUX: setup U3_34XX_GPIO61 (0xd80020c8): 0x0118 -> 0x011c
MUX: setup AH14_34XX_GPIO21 (0xd80025ea): 0x0100 -> 0x011c
MUX: setup AA10_3430_USB2HS_PHY_STP (0xd80025f2): 0x0100 -> 0x0003
MUX: setup AA8_3430_USB2HS_PHY_CLK (0xd80025f0): 0x0100 -> 0x0003
MUX: setup AA9_3430_USB2HS_PHY_DIR (0xd80025f4): 0x0100 -> 0x010b
MUX: setup AB11_3430_USB2HS_PHY_NXT (0xd80025f6): 0x0100 -> 0x010b
MUX: setup AB10_3430_USB2HS_PHY_D0 (0xd80025f8): 0x0100 -> 0x010b
MUX: setup AB9_3430_USB2HS_PHY_D1 (0xd80025fa): 0x0100 -> 0x010b
MUX: setup W3_3430_USB2HS_PHY_D2 (0xd80021d4): 0x0108 -> 0x010b
MUX: setup T4_3430_USB2HS_PHY_D3 (0xd80021de): 0x0108 -> 0x010b
MUX: setup T3_3430_USB2HS_PHY_D4 (0xd80021d8): 0x0100 -> 0x010b
MUX: setup R3_3430_USB2HS_PHY_D5 (0xd80021da): 0x0100 -> 0x010b
MUX: setup R4_3430_USB2HS_PHY_D6 (0xd80021dc): 0x0108 -> 0x010b
MUX: setup T2_3430_USB2HS_PHY_D7 (0xd80021d6): 0x0100 -> 0x010b
twl4030: client 1 is not initialized
MUX: setup AA21_34XX_GPIO157 (0xd800218e): 0x0018 -> 0x011c
MUX: setup C23_34XX_GPIO98 (0xd8002114): 0x0004 -> 0x011c
omap3evmdc: Driver registration complete
Switched to new clocking rate (Crystal/Core/MPU): 26.0/332/600 MHz
IVA2 clocking rate: 430 MHz
Calibrating delay loop... 597.64 BogoMIPS (lpj=2334720)
OMAP DMA hardware revision 4.0
USB: No board-specific platform config found
OMAP DSS rev 2.0
OMAP DISPC rev 3.0
OMAP VENC rev 2
OMAP DSI rev 1.0
bio: create slab <bio-0> at 0
i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz
twl4030: PIH (irq 7) chaining IRQs 368..375
twl4030: power (irq 373) chaining IRQs 376..383
twl4030: gpio (irq 368) chaining IRQs 384..401
i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
musb_hdrc: version 6.0, musb-dma, host, debug=0
HS USB OTG: revision 0x33, sysconfig 0x2011, sysstatus 0x1, intrfsel 0x1, simenable 0x0
musb_hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine (X), bulk split (X), HB-ISO Rx (X), HB-ISO Tx (X), SoftConn)
musb_hdrc: MHDRC RTL version 1.400
musb_hdrc: setup fifo_mode 4
musb_hdrc: 29/31 max ep, 16384/16384 memory
musb_hdrc: hw_ep 0shared, max 64
musb_hdrc: hw_ep 1tx, max 512
musb_hdrc: hw_ep 1rx, max 512
musb_hdrc: hw_ep 2tx, max 512
musb_hdrc: hw_ep 2rx, max 512
musb_hdrc: hw_ep 3tx, max 512
musb_hdrc: hw_ep 3rx, max 512
musb_hdrc: hw_ep 4tx, max 512
musb_hdrc: hw_ep 4rx, max 512
musb_hdrc: hw_ep 5tx, max 512
musb_hdrc: hw_ep 5rx, max 512
musb_hdrc: hw_ep 6tx, max 512
musb_hdrc: hw_ep 6rx, max 512
musb_hdrc: hw_ep 7tx, max 512
musb_hdrc: hw_ep 7rx, max 512
musb_hdrc: hw_ep 8tx, max 512
musb_hdrc: hw_ep 8rx, max 64
musb_hdrc: hw_ep 9tx, max 512
musb_hdrc: hw_ep 9rx, max 64
musb_hdrc: hw_ep 10tx, max 512
musb_hdrc: hw_ep 10rx, max 64
musb_hdrc: hw_ep 11tx, max 256
musb_hdrc: hw_ep 11rx, max 256
musb_hdrc: hw_ep 12tx, max 256
musb_hdrc: hw_ep 12rx, max 256
musb_hdrc: hw_ep 13tx, max 256
musb_hdrc: hw_ep 13rx, max 4096
musb_hdrc: hw_ep 14shared, max 1024
musb_hdrc: hw_ep 15shared, max 1024
musb_hdrc: USB Host mode controller at d80ab000 using DMA, IRQ 92
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.29-rc3-omap1 musb-hcd
usb usb1: SerialNumber: musb_hdrc
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Registered /proc/driver/musb_hdrc
NET: Registered protocol family 2
Switched to high resolution mode on CPU 0
IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP reno registered
NET: Registered protocol family 1
OMAP35x Linux PSP version 02.01.03.11 (OMAP3EVM)
NetWinder Floating Point Emulator V0.97 (double precision)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 441
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler anticipatory registered (default)
io scheduler deadline registered
io scheduler cfq registered
Generic Backlight Driver Initialized.
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
console [ttyS0] enabled
serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
brd: module loaded
loop: module loaded
smsc911x: Driver version 2008-10-21.
smsc911x-mdio: probed
eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=ffffffff:01, irq=-1)
net eth0: MAC Address: 00:50:c2:7e:98:67
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v0.1.0)
i2c /dev entries driver
Driver 'sd' needs updating - please use bus_type methods
omap2-nand driver initializing
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-bit)
Creating 5 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000080000 : "xloader-nand"
0x000000080000-0x000000240000 : "uboot-nand"
0x000000240000-0x000000280000 : "params-nand"
0x000000280000-0x000000780000 : "linux-nand"
0x000000780000-0x000010000000 : "jffs2-nand"
OneNAND driver initializing
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 2
ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: OMAP-EHCI Host Controller
usb usb2: Manufacturer: Linux 2.6.29-rc3-omap1 ehci_hcd
usb usb2: SerialNumber: ehci-omap.0
usb usb2: configuration #1 chosen from 1 choice
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 3 ports detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
input: omap_twl4030keypad as /class/input/input0
ads7846 spi1.0: touchscreen, irq 335
input: ADS784x Touchscreen as /class/input/input1
OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
cpuidle: using governor ladder
cpuidle: using governor menu
usbcore: registered new interface driver usbhid
usbhid: v2.6:USB HID core driver
Advanced Linux Sound Architecture Driver Version 1.0.19.
usbcore: registered new interface driver snd-usb-audio
No device for DAI twl4030
No device for DAI twl4030 Voice
No device for DAI omap-mcbsp-dai-0
No device for DAI omap-mcbsp-dai-1
No device for DAI omap-mcbsp-dai-2
No device for DAI omap-mcbsp-dai-3
No device for DAI omap-mcbsp-dai-4
OMAP3 EVM SoC init
TWL4030 Audio Codec init
asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok
ALSA device list:
#0: omap3evm (twl4030)
TCP cubic registered
NET: Registered protocol family 17
NET: Registered protocol family 15
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
Power Management for TI OMAP3.
SmartReflex driver initialized
Disabling unused clock "sr2_fck"
Disabling unused clock "sr1_fck"
Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_ick"
Disabling unused clock "gpt2_ick"
Disabling unused clock "gpt3_ick"
Disabling unused clock "gpt4_ick"
Disabling unused clock "gpt5_ick"
Disabling unused clock "gpt6_ick"
Disabling unused clock "gpt7_ick"
Disabling unused clock "gpt8_ick"
Disabling unused clock "gpt9_ick"
Disabling unused clock "wdt3_ick"
Disabling unused clock "wdt3_fck"
Disabling unused clock "gpio2_dbck"
Disabling unused clock "gpio3_dbck"
Disabling unused clock "gpio4_dbck"
Disabling unused clock "gpio5_dbck"
Disabling unused clock "gpt9_fck"
Disabling unused clock "gpt8_fck"
Disabling unused clock "gpt7_fck"
Disabling unused clock "gpt6_fck"
Disabling unused clock "gpt5_fck"
Disabling unused clock "gpt4_fck"
Disabling unused clock "gpt3_fck"
Disabling unused clock "gpt2_fck"
Disabling unused clock "gpt12_ick"
Disabling unused clock "wdt1_ick"
Disabling unused clock "wdt2_ick"
Disabling unused clock "wdt2_fck"
Disabling unused clock "gpio1_dbck"
Disabling unused clock "des1_ick"
Disabling unused clock "sha11_ick"
Disabling unused clock "rng_ick"
Disabling unused clock "aes1_ick"
Disabling unused clock "ssi_ick"
Disabling unused clock "mailboxes_ick"
Disabling unused clock "gpt10_ick"
Disabling unused clock "gpt11_ick"
Disabling unused clock "hdq_ick"
Disabling unused clock "mspro_ick"
Disabling unused clock "des2_ick"
Disabling unused clock "sha12_ick"
Disabling unused clock "aes2_ick"
Disabling unused clock "icr_ick"
Disabling unused clock "pka_ick"
Disabling unused clock "ssi_ssr_fck"
Disabling unused clock "hdq_fck"
Disabling unused clock "mspro_fck"
Disabling unused clock "gpt11_fck"
Disabling unused clock "sad2d_ick"
Disabling unused clock "dpll4_m6x2_ck"
Disabling unused clock "dpll3_m3x2_ck"
Disabling unused clock "sys_clkout1"
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
GPIO-153 autorequested
omap-dss DISPC error: Requested pixel clock not possible with the current OMAP2_DSS_MIN_FCK_PER_PCK setting. Turning the constraint off.
omap-dss: Could not find exact pixel clock. Requested 25190 kHz, got 25189 kHz
Display already enabled
Buffer Size = 3686400
omap_vout: registered and initialized video device 0 [v4l2]
omap_vout: registered and initialized video device 1 [v4l2]
display->updated
net eth0: SMSC911x/921x identified at 0xd085c000, IRQ: 336
Sending DHCP requests .., OK
IP-Config: Got DHCP answer from 192.168.1.100, my address is 192.168.1.10
IP-Config: Complete:
device=eth0, addr=192.168.1.10, mask=255.255.255.0, gw=192.168.1.1,
host=192.168.1.10, domain=, nis-domain=(none),
bootserver=192.168.1.100, rootserver=192.168.1.100, rootpath=/home/won/workdir/filesys
Looking up port of RPC 100003/2 on 192.168.1.100
Looking up port of RPC 100005/1 on 192.168.1.100
VFS: Mounted root (nfs filesystem) on device 0:12.
Freeing init memory: 156K
udev: starting version 141
udev: deprecated sysfs layout; update the kernel or disable CONFIG_SYSFS_DEPRECATED; some udev features will not work correctly
omap-dss: Could not find exact pixel clock. Requested 25189 kHz, got 25188 kHz
omap-dss: Could not find exact pixel clock. Requested 25188 kHz, got 25187 kHz