• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » OMAP™ Processors » OMAP35x Processors Forum » omap3530 tv out
Share
OMAP™ Processors
  • Forums
  • Announcements
Options
  • Subscribe via RSS
Resources
  • OMAP-L1x DSP+ARM9™-based Processors Product Folder
  • OMAP3525/30 DSP+ARM Cortex™-A8-based SOCs Product Folder

  • Top OMAPL Wiki Links
  • OMAPL3x Schematic Review Checklist
  • OMAPL13x Boot resources

  • OMAPL Document Resources
  • OMAPL137 Technical reference manual
  • OMAPL138 Technical reference manual
  • OMAPL Boot loader App Notes
  • Forums

    omap3530 tv out

    This question is not answered
    devakumar Jayavelu
    Posted by devakumar Jayavelu
    on Feb 19 2010 01:56 AM
    Prodigy110 points

    i have configured tvout and tested using background and color bar output(both pal and nstc).

    but while using dss digital output for tvout , output at tv is not proper. i am suspecting the problem with frame buffer address 1(DISPC_GFX_BA1).

    i am using 640x480 at dss config and 720x482 at digi config for nstc output.

    venc configs are done as mentioned in datasheet.

    the output at tv is distorted in this case.

    how i have to set DISPC_GFX_BA1 register and the description of  internal buffer usage in this(interlaced mode).

    tv out in omap3530
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    All Replies
    • Steve Clynes
      Posted by Steve Clynes
      on Feb 19 2010 14:28 PM
      Mastermind22890 points

      Devakumar,

      Are you doing this under an OS or directly through register access?

      The TV out resolution needs to be either 720x480 for NTSC or 720x576 for PAL. If your frame buffer is of a different resolution then you must either use a video pipe and scale, or crop/clip the image to fit.

      Both these require more than just changing the BA registers.

      Have a look at the following wiki article for information on how the frame buffers, pipes and outputs can be configured.

      http://wiki.omap.com/index.php/Display_Subsystem

      (http://wiki.omap.com/index.php?title=Category:OMAP35x may also be useful to you)

      If you are working under Linux, which build are you using? You should be able to enable the tvout through V4L2/fbdev/ioctls without the need for direct register accesses.

      If you are not using an OS and accessing the registers directly then I can send you some simple sample code which access the registers directly for video, graphics, scaled, non-scaled, LCD, TV etc....

      BR,

      Steve

      Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • devakumar Jayavelu
      Posted by devakumar Jayavelu
      on Feb 22 2010 00:23 AM
      Prodigy110 points

      i am using it in bios (direct access).

      my intention is to use a standard image(ex: 640x480 image is dumped as an continuous array at a same location in all cases) for both vga/lcd and tvout, and by changing  DISPC_GFX_ATTRIBUTES[8]: GFXCHANNELOUT i should able to switch between TV and VGA/LCD. is it possible?

      i hope configuration for tvout register(VENC for pal and nstc) are same as in the omap3530 datasheet (please mention if any changes required).

      i am totally confused with BA1 register.

      as per my understanding BA1 is used only in case of TVOUT(GFXCHANNELOUT set to 1), its used for getting odd line data of interlaced mode.

      doubt: is it must to dump the oddline data in a separate buffer? or i can load BA1 with BA0+size of one line data?

      if it is "BA0+size of one line data" then how internally it will use it to access next odd line data (even line as well)?

      is it possible to have TVOUT and VGA/LCD at same time(with same output)?

      which are the registers in DISPC have effect over TVOUT.

      expecting some sample code as u mentioned.

      thanks and regards.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Steve Clynes
      Posted by Steve Clynes
      on Feb 22 2010 09:33 AM
      Mastermind22890 points

      There are a number of ways you can do this. It is even possible to have both active at the same time (as you can see from the Wiki page I mentioned).

      For the TV out, there are a few things you need to do. If the source image is 640x480 then you need to either scale it to fit 720x480 or window the image on the 720x480 output necessary for NTSC (For PAL the size is 720x576).

      Regarding the BA registers, for the TV out you need to configure BA1 to point to the start of the image and BA0 to point to the start of the second line. Then, the line step registers need to be set to (640xpixel size) so that each field will skip alternate lines.

      If you want to scale the image to fit, then you need to use a video pipe and not a graphics pipe.

      One thing to note with most TVs... They will usually clip the outer 10% so that you will not see anything on the very top, bottom, left or right. Some TVs do more than 10%, some do less, but 10% is a good approximation.

      To avoid this you may want to actually scale your image down for the TV out and center it on the output display.

      e-mail me at sclynes@ti.com and I will send you some sample code to help you.

      BR,

      Steve

      Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • devakumar Jayavelu
      Posted by devakumar Jayavelu
      on Feb 22 2010 23:27 PM
      Prodigy110 points

      thanks Steve.

      now its fine. but i faced small flicker in NSTC mode(with typical configuration as in data sheet), then used the settings for NSTC from some reference code and solved it.

      also in above reply,

      Regarding the BA registers, for the TV out you need to configure BA1 to point to the start of the image and BA0 to point to the start of the second line. 

      is it correct or is it like this?

      Regarding the BA registers, for the TV out you need to configure BA0 to point to the start of the image and BA1 to point to the start of the second line. 

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Steve Clynes
      Posted by Steve Clynes
      on Feb 23 2010 08:48 AM
      Mastermind22890 points

      It should be the first one :)

      Here is a snippet from my code example...

          WritePhysical(DISPC_VID1_BA1  + VidOffset, (unsigned int)Attributes.Buffer.BufferPtrs.PtrPBuffer + BufferOffset);
          WritePhysical(DISPC_VID1_BA0  + VidOffset, (unsigned int)Attributes.Buffer.BufferPtrs.PtrPBuffer + BufferOffset + ((Attributes.Buffer.Width * BPP / 8)));

      BR,

      Steve

      Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • sairam
      Posted by sairam
      on Jul 13 2010 04:25 AM
      Prodigy150 points

      Hi Devakumar ,

       

      Please share the reference code to solve the flicker issue for OMAP NTSC TV OUT .

       

       

      regards,

      Sairam.S

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • imtiyaj
      Posted by imtiyaj
      on Nov 15 2010 06:01 AM
      Prodigy240 points

      Hello Steve,

      I am drawing(actually Android / Qt) some graphics on to the Graphics overlay and displaying on a TV, and running Linux 2.6.32 kernel. The mode argument for kernel commandline is "tv:ntsc".  I have the use case of Graphics and Video overlay blending while video playback happens.

      1. The problem is that  the graphics, video always seem to be cropped from left, right , top and bottom while in TV mode. This does not happen when I configure it to use VGA display. I am relating this to what, you have said in earlier mail, that the TVs usually clip the outer 10%. 

      What would you suggest seeing the use-case and OS scenario?

       

      2. Is it possible to display both on TV and VGA at the same time, considering that I have to blend video and graphics while playing videos?

      What approach, would you suggest in this case?

      I have tried somethings on my side before writing here to seek guidance. I have tried to modify the xres and yres in the omap_dss_ntsc_timings structure in venc.c to bring down the resolution to some value that fits within the TV screen. But not all combinations of xres and yres are OK, as I get "Out of Sync" error for most of the new values of xres and yres which I try.

      Also did some modifications to VENC registers, but don't know how to arrive on the set of values which are correct to fit the Graphics on to TV. Can you point me to some document, which explains this in detail?

      Thanking you in advance and wating for your inputs,

      regards

      -Nitin

       

       

       

       

       

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Steve Clynes
      Posted by Steve Clynes
      on Nov 15 2010 09:29 AM
      Mastermind22890 points

      Nitin,

      Sorry you are having trouble. Overscan is always an issue since not all TVs perform it and you cannot ever really be sure just how much a particular TV will do.

      There are 2 options to correct for this TV induced overscan.

      1) Reduce your source image size to about 640 x 425 then center it on the TV out.
      2) Scale your source image down to about 640 x 425 then center it on the TV out.

      Option 1 is the simplest and most efficient in terms of memory bandwidth but obviously reduces your active frame buffer area.

      Option 2 will end up doubling the memory bandwidth requirements since vertical scaling of an interlaced image requires 2x image reading. This option will, however, allow you to view your entire original frame buffer.

      I will have to defer to folks who know more than me regarding the linux drivers and the current options for scaling through the Linux OS & drivers.

      I have attached some register level configuration code which may help if you want to access the hardware directly. Be aware though that this code is very much development code and therefore should really only be used to help describe how the registers behave.

      BR,

      Steve

      3554.LCD_TV.zip

      Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • imtiyaj
      Posted by imtiyaj
      on Nov 16 2010 08:30 AM
      Prodigy240 points

      Hello Steve,

      Thanks for the inputs. 

      I did try the following things today and also attaching the images of how my TV screen looks and hows the Graphics still getting cut from left and top side. Before doing this experiment I had changed the values of VENC registers to those sent by you in the previous code. After that I modified some of the register values, which I will mention below.

      I wrote 720, 480/2 to the DISPC_SIZE_DIG. I allocated frame-buffer of size 684x456 and generated graphics of same size and wrote it to the framebuffer. I think, thats what the code you sent is trying to do(though it uses a 640x480 image).

      Please let me know if this approach is correct. These are my VENC register values finally and the pictures which I am sending you correspond to these values.

      Is there a document TI specific or general which you can point me to , which will help me understand the significance if these registers and terminology in more detail and what effect their values have on screen size? What is Hsync internal Vs Hsync external ?

       

               .f_control                              = 0,

              .vidout_ctrl                            = 0,

              .sync_ctrl                              = 0x8040, //RBee

              .llen                                   = 0x359,

              .flens                                  = 0x20C,

              .hfltr_ctrl                             = 0,

              .cc_carr_wss_carr                       = 0x043F0000,

              .c_phase                                = 0,

              .gain_u                                 = 0x102,

              .gain_v                                 = 0x16C,

              .gain_y                                 = 0x12F,

              .black_level                            = 0x43,

              .blank_level                            = 0x38,

              .x_color                                = 0x7,

              .m_control                              = 0x1,

              .bstamp_wss_data                        = 0x38,

              .s_carr                                 = 0x21F07C1F,

              .line21                                 = 0,

              .ln_sel                                 = 0x00000015,

              .l21__wc_ctl                            = 0x00001400,

              .htrigger_vtrigger                      = 0,

              .savid__eavid                           = 0x069300F4,

              .flen__fal                              = 0x0016020C,

              .lal__phase_reset                       = 0x00060107,

              .hs_int_start_stop_x                    = 0x008D034E, //RBee

              .hs_ext_start_stop_x                    = 0x000F0359,

               .vs_int_start_x                         = 0x01A00000,

              .vs_int_stop_x__vs_int_start_y          = 0x020301A0,

              .vs_int_stop_y__vs_ext_start_x          = 0x01AC0024,

              .vs_ext_stop_x__vs_ext_start_y          = 0x020D01AC,

              .vs_ext_stop_y                          = 0x00000006,

              .avid_start_stop_x                      = 0x03480078,

              .avid_start_stop_y                      = 0x02040024,

              .fid_int_start_x__fid_int_start_y       = 0x0001008A,

              .fid_int_offset_y__fid_ext_start_x      = 0x01AC0106,

              .fid_ext_start_y__fid_ext_offset_y      = 0x01060006,

       

              .tvdetgp_int_start_stop_x               = 0x00140001,

              .tvdetgp_int_start_stop_y               = 0x00010001,

              .gen_ctrl                               = 0x00F90000,

      Please correct me if there is some thing wrong in my approach..

      Thanks and regards

      -Nitin

       

       

       

       

       

       

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Steve Clynes
      Posted by Steve Clynes
      on Nov 16 2010 09:15 AM
      Mastermind22890 points

      I suggest that you also look at the following wiki page which explains what the hardware capabilities are. You might find that this makes things a lot clearer.

      http://processors.wiki.ti.com/index.php/Display_Subsystem

      Simply reducing the frame buffer image size will not move its position, only its size. You also need to move the output image to the right and down. This is done through the graphics pipe control registers.

      Do not make any changes to the TV out VENC settings. These MUST be as I sent in the example code in order to generate a standard NTSC video signal.

      The register you need to touch, in your case for the graphics pipe, is DISPC_GFX_POSITION (0x48050488)

      If your new frame buffer is 684 then in order to center your image you need to set the x position to be (720-684) / 2 = 18

      Vertically set the y position to be (480-456) / 2 = 12

      BR,

      Steve

      Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • imtiyaj
      Posted by imtiyaj
      on Nov 16 2010 10:21 AM
      Prodigy240 points

      Thanks Steve to clarify... I will check it.

       

      regards

      Nitin

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • j-breeze
      Posted by j-breeze
      on May 23 2011 03:29 AM
      Expert1670 points

      Hi, Steve-san

      My Customer has the similar TV out problems using VID2.

      Customer conditions are:
        - Source Image Size  = 800x480
        - Display Size              = 720x482 (NTSC)
        - Destination Size       = 684x458 (90% NTSC)  ...Case-1
                                               = 648x434 (80% NTSC)  ...Case-2
        - Not changed VENC settings, same as Technical Reference Manual(spruf98r) table 15-69 Video Encoder Register Programming Values.
        - PRCM regs settings
            (0x48004e00)PRCM.CM_FCLKEN_DSS    =0x00000007
            (0x48004d00)PRCM.CM_CLKEN_PLL       =0x80371037
            (0x48004d30)PRCM.CM_AUTOIDLE_PLL =0x00000009
            (0x48004d40)PRCM.CM_CLKSEL1_PLL   =0x094c0c00
            (0x48004e40)PRCM.CM_CLKSEL_DSS    =0x00001002

      ~~~~~~~~~~~~~~
      o Case-1 Trouble
      ~~~~~~~~~~~~~~

        - SYNCLOSTDIGITAL occured.
        - Display becomes black.

      ~~~~~~~~~~~~~~
      o Case-2 Trouble
      ~~~~~~~~~~~~~~

        When customer sets the X position to be (720-648) / 2 = 36 and y position to be (482-434) / 2 = 24:

        - SYNCLOSTDIGITAL occured.
        - Display becomes black.

           (*) Same as Case-1

        When customer sets the X position to be  > 13 and y position to be >10:

        - SYNCLOSTDIGITAL occured.
        - Display becomes black.

           (*) Same as Case-1

        When customer sets the X position to be  < 13 and y position to be < 10:

        - Down-sampling established
        - Not centered the dawn-sampling image because x/y positions is not correct.

      In Case-1/2, are there any down-sampling lmitations like LCD out described in errata(sprz278f) 2.1.20? 

      Thanks in advance for your cooperation.

      Best regards,
      j-breeze

      omap3530 TV out resize downsampling
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • suhas m1
      Posted by suhas m1
      on Mar 30 2013 09:49 AM
      Intellectual890 points

      hi steve,

      we r able to get the DM3730 display on TV using its TVOUT signals... but TVOUT signal stops coming if the LCD driver is configured for a resolution  greater than 800*600....so what might be the problem???

      we want to use the TV out @ 1024*768 resolution since our LCD panel resolution is 1024*768..... since we want to display on  both tvout n lcd simultaneously

      thnx u in advance ......

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • suhas m1
      Posted by suhas m1
      on Apr 05 2013 00:10 AM
      Intellectual890 points

      hi Steve, here is my DSS register dump......for 1024*600 resolution..... but no signal on tv..tv is blank...

      DSS Registers:
      DSS_REVISIONNUMBER=0x00000020
      DSS_SYSCONFIG=0x00000001
      DSS_SYSSTATUS=0x00000001
      DSS_CONTROL=0x00000038
      DSS_SDI_CONTROL=0x00000000
      DSS_PLL_CONTROL=0x00000000
      DSS_SDI_STATUS=0x00000081
       
      DISPC Registers:
      DISPC_REVISION=0x00000030
      DISPC_SYSCONFIG=0x00001009
      DISPC_SYSSTATUS=0x00000001
      DISPC_IRQSTATUS=0x000081AE
      DISPC_IRQENABLE=0x00005240
       
      DISPC Registers (Control):
      DISPC_CONTROL=0x0801830B
      DISPC_CONFIG=0x00000208
      DISPC_CAPABLE=0x000003FF
      DISPC_DEFAULT_COLOR0=0x00000000
      DISPC_DEFAULT_COLOR1=0x00000000
      DISPC_TRANS_COLOR0=0x00000000
      DISPC_TRANS_COLOR1=0x00000000
      DISPC_GLOBAL_ALPHA=0x00FF00FF
       
      DISPC Registers (LCD):
      DISPC_LINE_STATUS=0x0000013B
      DISPC_LINE_NUMBER=0x00000000
      DISPC_TIMING_H=0x0780C801
      DISPC_TIMING_V=0x00F01400
      DISPC_POL_FREQ=0x00023000
      DISPC_DIVISOR=0x00010001
      DISPC_SIZE_DIG=0x012002CF
      DISPC_SIZE_LCD=0x025703FF
       
      DISPC Registers (GFX):
      DISPC_GFX_BA0=0x82802000
      DISPC_GFX_BA1=0x82802000
      DISPC_GFX_POSITION=0x00000000
      DISPC_GFX_SIZE=0x025703FF
      DISPC_GFX_ATTRIBUTES=0x000000AD
      DISPC_GFX_FIFO_THRESHOLD=0x03FF01FF
      DISPC_GFX_FIFO_SIZE_STATUS=0x00000400
      DISPC_GFX_ROW_INC=0x00000001
      DISPC_GFX_PIXEL_INC=0x00000001
      DISPC_GFX_WINDOW_SKIP=0x00000000
      DISPC_GFX_TABLE_BA=0x89A62000
       
      DISPC Registers (VID 1):
      BA0=0x00000000
      BA1=0x00000000
      POSITION=0x00000000
      SIZE=0x00000000
      ATTRIBUTES=0x00000000
      FIFO_THRESHOLD=0x03FF03C0
      FIFO_SIZE_STATUS=0x00000400
      ROW_INC=0x00000001
      PIXEL_INC=0x00000001
      FIR=0x00000000
      PICTURE_SIZE=0x00000000
      ACCU0=0x00000000
      ACCU1=0x00000000
      DISPC_VIDn_FIR_COEF_Hi _HVi _Vi:
         0: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         1: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         2: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         3: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         4: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         5: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         6: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         7: H = 0x00000000   HV = 0x00000000   V = 0x00000000
      CONV_COEF0=0x00000000
      CONV_COEF1=0x00000000
      CONV_COEF2=0x00000000
      CONV_COEF3=0x00000000
      CONV_COEF4=0x00000000
       
      DISPC Registers (VID 2):
      BA0=0x82802800
      BA1=0x82802000
      POSITION=0x002A002C
      SIZE=0x00C90287
      ATTRIBUTES=0x006183ED
      FIFO_THRESHOLD=0x03FF01FF
      FIFO_SIZE_STATUS=0x00000400
      ROW_INC=0x00000001
      PIXEL_INC=0x00000001
      FIR=0x0BE10652
      PICTURE_SIZE=0x025703FF
      ACCU0=0x01F00000
      ACCU1=0x00000000
      DISPC_VIDn_FIR_COEF_Hi _HVi _Vi:
         0: H = 0x1b761bea   HV = 0x243624ea   V = 0x00000101
         1: H = 0x2b730dee   HV = 0x28371fe7   V = 0x000004fe
         2: H = 0x3a6b00f4   HV = 0x2c361be7   V = 0x000008fb
         3: H = 0x475ff6fa   HV = 0x303516ea   V = 0x00000df8
         4: H = 0xef5151ef   HV = 0x12333300   V = 0x0000f612
         5: H = 0xf65f47ea   HV = 0x163530fa   V = 0x0000f80d
         6: H = 0x006b3ae7   HV = 0x1b362cf4   V = 0x0000fb08
         7: H = 0x0d732be7   HV = 0x1f3728ee   V = 0x0000fe04
      CONV_COEF0=0x0199012A
      CONV_COEF1=0x012A0000
      CONV_COEF2=0x079C0730
      CONV_COEF3=0x0000012A
      CONV_COEF4=0x00000205

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • suhas m1
      Posted by suhas m1
      on Apr 05 2013 00:12 AM
      Intellectual890 points

      hi Steve....

      i thought it will be helpful if i post a register dump for 800*600 resolution..... with 800*600 resolution my tv out signal is coming... im able display on tv... below is the tested n working register dump for 800*600 resolution....... pls try to compare both....and suggest me a solution...

      DSS Registers:
      DSS_REVISIONNUMBER=0x00000020
      DSS_SYSCONFIG=0x00000001
      DSS_SYSSTATUS=0x00000001
      DSS_CONTROL=0x00000038
      DSS_SDI_CONTROL=0x00000000
      DSS_PLL_CONTROL=0x00000000
      DSS_SDI_STATUS=0x00000081
       
      DISPC Registers:
      DISPC_REVISION=0x00000030
      DISPC_SYSCONFIG=0x00001009
      DISPC_SYSSTATUS=0x00000001
      DISPC_IRQSTATUS=0x0000A1AE
      DISPC_IRQENABLE=0x00005240
       
      DISPC Registers (Control):
      DISPC_CONTROL=0x0801830B
      DISPC_CONFIG=0x00000208
      DISPC_CAPABLE=0x000003FF
      DISPC_DEFAULT_COLOR0=0x00000000
      DISPC_DEFAULT_COLOR1=0x00000000
      DISPC_TRANS_COLOR0=0x00000000
      DISPC_TRANS_COLOR1=0x00000000
      DISPC_GLOBAL_ALPHA=0x00FF00FF
       
      DISPC Registers (LCD):
      DISPC_LINE_STATUS=0x0000014F
      DISPC_LINE_NUMBER=0x00000000
      DISPC_TIMING_H=0x0970273F
      DISPC_TIMING_V=0x01700103
      DISPC_POL_FREQ=0x00020000
      DISPC_DIVISOR=0x00010002
      DISPC_SIZE_DIG=0x012002CF
      DISPC_SIZE_LCD=0x0257031F
       
      DISPC Registers (GFX):
      DISPC_GFX_BA0=0x82802000
      DISPC_GFX_BA1=0x82802000
      DISPC_GFX_POSITION=0x00000000
      DISPC_GFX_SIZE=0x0257031F
      DISPC_GFX_ATTRIBUTES=0x000000AD
      DISPC_GFX_FIFO_THRESHOLD=0x03FF01FF
      DISPC_GFX_FIFO_SIZE_STATUS=0x00000400
      DISPC_GFX_ROW_INC=0x00000001
      DISPC_GFX_PIXEL_INC=0x00000001
      DISPC_GFX_WINDOW_SKIP=0x00000000
      DISPC_GFX_TABLE_BA=0x89A86000
       
      DISPC Registers (VID 1):
      BA0=0x00000000
      BA1=0x00000000
      POSITION=0x00000000
      SIZE=0x00000000
      ATTRIBUTES=0x00000000
      FIFO_THRESHOLD=0x03FF03C0
      FIFO_SIZE_STATUS=0x00000400
      ROW_INC=0x00000001
      PIXEL_INC=0x00000001
      FIR=0x00000000
      PICTURE_SIZE=0x00000000
      ACCU0=0x00000000
      ACCU1=0x00000000
      DISPC_VIDn_FIR_COEF_Hi _HVi _Vi:
         0: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         1: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         2: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         3: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         4: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         5: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         6: H = 0x00000000   HV = 0x00000000   V = 0x00000000
         7: H = 0x00000000   HV = 0x00000000   V = 0x00000000
      CONV_COEF0=0x00000000
      CONV_COEF1=0x00000000
      CONV_COEF2=0x00000000
      CONV_COEF3=0x00000000
      CONV_COEF4=0x00000000
       
      DISPC Registers (VID 2):
      BA0=0x82802640
      BA1=0x82802000
      POSITION=0x000E002C
      SIZE=0x01020287
      ATTRIBUTES=0x006183ED
      FIFO_THRESHOLD=0x03FF01FF
      FIFO_SIZE_STATUS=0x00000400
      ROW_INC=0x00000001
      PIXEL_INC=0x00000001
      FIR=0x094404F0
      PICTURE_SIZE=0x0257031F
      ACCU0=0x00A20000
      ACCU1=0x00000000
      DISPC_VIDn_FIR_COEF_Hi _HVi _Vi:
         0: H = 0x028002fe   HV = 0x264c26fe   V = 0x0000f4f4
         1: H = 0x147df405   HV = 0x2f481ff6   V = 0x0000f8f2
         2: H = 0x2974ea0b   HV = 0x354916ee   V = 0x0000fcf0
         3: H = 0x3e66e50f   HV = 0x3b450fe8   V = 0x000001f0
         4: H = 0xe45353e4   HV = 0x08404012   V = 0x0000f008
         5: H = 0xe5663ee8   HV = 0x0f453b0f   V = 0x0000f001
         6: H = 0xea7429ee   HV = 0x1649350b   V = 0x0000f0fc
         7: H = 0xf47d14f6   HV = 0x1f482f05   V = 0x0000f3f7
      CONV_COEF0=0x0199012A
      CONV_COEF1=0x012A0000
      CONV_COEF2=0x079C0730
      CONV_COEF3=0x0000012A
      CONV_COEF4=0x00000205

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    TI E2E™ Community
    • Support Forums
    • Blogs
    • Videos
    • Groups
    • Site Support & Feedback
    • Settings
    TI E2E™ Community Groups
    • TI University Program
    • Make the Switch
    • Microcontroller Projects
    • Motor Drive & Control
    Other Communities
    • Deyisupport
    • Designsomething.org
    • beagleboard.org
    • TI on Element 14
    • TI on TechXchangeSM
    Other Technical & Support Resources
    • WEBENCH® Design Center
    • Product Information Centers
    • Technical Documents
    • TI Design Network
    • TI Technical Articles
    • TI Training

    All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

    Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

    Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
    TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

    TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
    embedded processors, along with software, tools and the industry’s largest sales/support staff.

    © Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
    Trademarks | Privacy Policy | Terms of Use