HI all
I have integrated the mpeg4 encoder with the codec server. But when i am running the it i am getting can not open encoder error
i run as :CE_DEBUG=2 ./app.xv5T
and the error is like below
ti.sdo.ce.video1.VIDDEC2 - VIDDEC2_create> Enter (engine=0x286d0, name='viddec2_copy', params=0x0) CV - VISA_create(0x286d0, 'mpeg4dec', 0x0, 0 x2484, 'ti.sdo.ce.video2.IVIDDEC2') CV - VISA_create2(0x286d0, 'mpeg4dec', 0x0, 0x0, 0x2484, 'ti.sdo.ce.video2.IVIDDEC2') CE - Engine_getConstName> Unable to locate alg " mpeg4dec" (type "ti.sdo.ce.video2.IVIDDEC2"). CV - VISA_create2> Unable to locate alg "mpeg4dec". I am using dvsdk_3_00_02_04/codec_engine_2_24 OMAP3530 processor
hi, Dipteswar
i'm facing with the same issue on our target board, i just want to know if you get your problem solved.
regards, Mike
Thanks.