Paul,
I am pretty new basically first time dealing with OMAP Processor and CCSv4.x . I tried to use your loopback example. It builds successfully, But However, it doesn't load program on target.
I got loopback example from : http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/p/52300/190150.aspx?PageIndex=2
Following are my development environment:
1. Mistral OMAP3530 EVM Rev G Board
2. CCSv4.x
3. Spectrum Digital USB 510 Plus JTAG Emulator
Thru Multi launcher I can boot the board it has Xloader 1.42 and U-Boot 2008.10.
I am trying to load the program thru CCSv4.x. I am able to connect the target but when I am trying to Debug Active Project it complains about in console.
TMS320C64XP: Error connecting to the target: Error 0x80000260/-1178 Fatal Error during: Execution, Initialization, OCS, The target does not have a CPU clock.
I am not sure where I am going wrong. is it somehting to do with setting up correct *.gel file or Target ocnfiguration file.. (*.cxml)...
Please would be able to tell me how you were able to load the program on target and debug it...?
Please any help would be appreciated.
Thanks,
AD