Hi All:
I am debugging the omap 3530 I2C module.
Questions as below :
1.when in Master Transmite mode.isr (interrupt),how to turn off the interrupt from the same source?
ie:registers I2C_STAT[4] I2C_STAT[14] bits?
2.if the register I2C_CON[15] is set to "0",when the previous status is "0".reset?
else if the register I2C_CON[15] is set to "1",when the previous status is "1", reset?