MIDAS Ultrasound v2.0 Demo (http://processors.wiki.ti.com/index.php/MIDAS_Ultrasound_v2.0_Demo#PSP_and_DVSDK.C2.A0Setup)
I try MIDAS Ultrasound V2.0 Demo on OMAP3530.
First, I try setup program PSP and DVSDK.
That site is GSG: OMAP35x DVEVM Software Setup (http://processors.wiki.ti.com/index.php/GSG:_OMAP35x_DVEVM_Software_Setup#Installing_the_software)
I follow this sit.
I try 5.3 Rebuilding the DVSDK software for the target.
and I try setup Rules.make & make all.
7. While in the same directory that contains Rules.make, use the following commands to build the DVSDK demo applications and put the resulting binaries on the target file system specified by EXEC_DIR.
host $ make clean host $ make all <-- I do it. host $ make install
start make all.
I get a error during the compile this.
My error message is
Linking interface from dec.o enc.o encdec.o main.o menu.o start.o tparty.o ../keypad.o ../uibuttons.o interface_config/linker.cmd..make[3]: Leaving directory `/home/won/dvsdk/dvsdk_3_01_00_06/dvsdk_demos_3_01_00_09/omap3530/interface'make[2]: Leaving directory `/home/won/dvsdk/dvsdk_3_01_00_06/dvsdk_demos_3_01_00_09/omap3530'make[1]: Leaving directory `/home/won/dvsdk/dvsdk_3_01_00_06/dvsdk_demos_3_01_00_09'make -C /home/won/dvsdk/dvsdk_3_01_00_06/dvtb_4_20_04 omap3530 CODECS=TSPAmake[1]: Entering directory `/home/won/dvsdk/dvsdk_3_01_00_06/dvtb_4_20_04'********************************************Building DVTB for omap3530...********************************************cd packages/ti/sdo/dvtb/omap3530/linux && make
make[2]: Entering directory `/home/won/dvsdk/dvsdk_3_01_00_06/dvtb_4_20_04/packages/ti/sdo/dvtb/omap3530/linux'
XDCPATH="/home/won/dvsdk/dvsdk_3_01_00_06/cs1omap3530_1_01_00 /packages;/home/won/dvsdk/dvsdk_3_01_00_06/framework_components_2_25_01_05/packages;/home/won/dvsdk/dvsdk_3_01_00_06/codec_engine_2_25_01_06/packages;/home/won/dvsdk/dvsdk_3_01_00_06/dsplink_linux_1_65_00_01/packages;/home/won/dvsdk/dvsdk_3_01_00_06/xdais_6_25_01_08/packages;/home/won/dvsdk/dvsdk_3_01_00_06/linuxutils_2_25_01_06/packages;/home/won/dvsdk/dvsdk_3_01_00_06/linuxlibs_3_01/include;/home/won/dvsdk/dvsdk_3_01_00_06/local_power_manager_linux_1_24_01/packages;/home/won/dvsdk/dvsdk_3_01_00_06/bios_5_41_00_06/packages;/home/won/dvsdk/dvsdk_3_01_00_06/bios_5_41_00_06/packages/ti/bios/include;/home/won/dvsdk/dvsdk_3_01_00_06/bios_5_41_00_06/packages;" /home/won/dvsdk/dvsdk_3_01_00_06/xdctools_3_16_01_27/xs xdc.tools.configuro -c /home/won/toolchain/arm-2008q1 -o dvtb_omap3530 -t gnu.targets.arm.GCArmv5T -p ti.platforms.evm3530 -b config.bld dvtb_omap3530.cfg/home/won/dvsdk/dvsdk_3_01_00_06/xdctools_3_16_01_27/packages/xdc/bld/xdc_rules.mak:161: *** The macro XDCPATH must not contain any spaces in pathnames. stop.
Warning: directory "/home/won/dvsdk/dvsdk_3_01_00_06/cs1omap3530_1_01_00 /packages" on package path does not existjs: "/home/won/dvsdk/dvsdk_3_01_00_06/xdctools_3_16_01_27/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
make[2]: *** [dvtb_omap3530] error 1
make[2]: Leaving directory `/home/won/dvsdk/dvsdk_3_01_00_06/dvtb_4_20_04/packages/ti/sdo/dvtb/omap3530/linux'
make[1]: *** [OMAP3530_BUILD] error 2
make[1]:/ti-ezsdk_dm816x-evm_5_01_01_80/xdctools_3_20_08_88
make: *** [dvtb] error 2
How can I correct this error.
Help me.