hi, all
I am running the linux-3.3.2 on my omap3 platform, then it hang on booting, the booting message stop at "Failed to open /dev/kmsg for logging: No such file or directory".
I use the following command to build the kernel:
make mrproper
make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm omap2plus_defconfig
make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm uImage
hope help...
the full booting message show as below:
Starting kernel ...
Uncompressing Linux... done, booting the kernel.[ 0.000000] Booting Linux on physical CPU 0[ 0.000000] Linux version 3.3.2 (qing@HAHA) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 SMP Mon Apr 16 092[ 0.000000] CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c53c7d[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT nonaliasing instruction cache[ 0.000000] Machine: OMAP3 Beagle Board[ 0.000000] Memory policy: ECC disabled, Data cache writeback[ 0.000000] OMAP3430/3530 ES3.1 (l2cache iva sgx neon isp )[ 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/332/500 MHz[ 0.000000] PERCPU: Embedded 8 pages/cpu @c0e1d000 s10880 r8192 d13696 u32768[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64768[ 0.000000] Kernel command line: console=ttyO2,115200n8 root=/dev/mtdblock4 rootfstype=jffs2[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)[ 0.000000] Memory: 255MB = 255MB total[ 0.000000] Memory: 246436k/246436k available, 15708k reserved, 0K highmem[ 0.000000] Virtual kernel memory layout:[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)[ 0.000000] .text : 0xc0008000 - 0xc05e6170 (6009 kB)[ 0.000000] .init : 0xc05e7000 - 0xc0634a80 ( 311 kB)[ 0.000000] .data : 0xc0636000 - 0xc06c1cd0 ( 560 kB)[ 0.000000] .bss : 0xc06c1cf4 - 0xc0c178dc (5463 kB)[ 0.000000] Hierarchical RCU implementation.[ 0.000000] NR_IRQS:474[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts[ 0.000000] Total of 96 interrupts on 1 active controller[ 0.000000] OMAP clockevent source: GPTIMER12 at 32768 Hz[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms[ 0.000000] Console: colour dummy device 80x30[ 0.000000] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar[ 0.000000] ... MAX_LOCKDEP_SUBCLASSES: 8[ 0.000000] ... MAX_LOCK_DEPTH: 48[ 0.000000] ... MAX_LOCKDEP_KEYS: 8191[ 0.000000] ... CLASSHASH_SIZE: 4096[ 0.000000] ... MAX_LOCKDEP_ENTRIES: 16384[ 0.000000] ... MAX_LOCKDEP_CHAINS: 32768[ 0.000000] ... CHAINHASH_SIZE: 16384[ 0.000000] memory used by lock dependency info: 3695 kB[ 0.000000] per task-struct memory footprint: 1152 bytes[ 0.001861] Calibrating delay loop... 490.52 BogoMIPS (lpj=1916928)[ 0.085388] pid_max: default: 32768 minimum: 301[ 0.087188] Security Framework initialized[ 0.087829] Mount-cache hash table entries: 512[ 0.098480] CPU: Testing write buffer coherency: ok[ 0.100799] CPU0: thread -1, cpu 0, socket -1, mpidr 0[ 0.101135] Setting up static identity map for 0x804439b8 - 0x80443a28[ 0.105926] Brought up 1 CPUs[ 0.105957] SMP: Total of 1 processors activated (490.52 BogoMIPS).[ 0.136840] omap_hwmod: usbtll_fck: missing clockdomain for usbtll_fck.[ 0.181030] print_constraints: dummy: [ 0.186004] NET: Registered protocol family 16[ 0.188934] GPMC revision 5.0[ 0.217163] gpiochip_add: registered GPIOs 0 to 31 on device: gpio[ 0.218841] OMAP GPIO hardware version 2.5[ 0.221435] gpiochip_add: registered GPIOs 32 to 63 on device: gpio[ 0.224639] gpiochip_add: registered GPIOs 64 to 95 on device: gpio[ 0.228210] gpiochip_add: registered GPIOs 96 to 127 on device: gpio[ 0.231384] gpiochip_add: registered GPIOs 128 to 159 on device: gpio[ 0.234985] gpiochip_add: registered GPIOs 160 to 191 on device: gpio[ 0.254638] omap_mux_init: Add partition: #1: core, flags: 0[ 0.259185] OMAP3 Beagle Rev: Ax/Bx[ 0.292785] Reprogramming SDRC clock to 332000000 Hz[ 0.295532] Found NAND on CS0[ 0.295593] Registering NAND on CS0[ 0.298339] Unable to get DVI reset GPIO[ 0.299316] hw-breakpoint: debug architecture 0x4 unsupported.[ 0.354980] omap-mcbsp.2: alias fck already exists[ 0.357727] omap-mcbsp.3: alias fck already exists[ 0.374389] OMAP DMA hardware revision 4.0[ 0.578063] bio: create slab <bio-0> at 0[ 0.602478] SCSI subsystem initialized[ 0.628845] usbcore: registered new interface driver usbfs[ 0.632568] usbcore: registered new interface driver hub[ 0.635101] usbcore: registered new device driver usb[ 0.642547] omap_i2c omap_i2c.1: bus 1 rev1.3.12 at 2600 kHz[ 0.666503] twl4030: PIH (irq 7) chaining IRQs 368..375[ 0.668273] twl4030: power (irq 373) chaining IRQs 376..383[ 0.673553] twl4030: gpio (irq 368) chaining IRQs 384..401[ 0.677368] gpiochip_add: registered GPIOs 192 to 211 on device: twl4030[ 0.701293] print_constraints: VMMC1: 1850 <--> 3150 mV at 3150 mV normal standby[ 0.707427] print_constraints: VDAC: 1800 mV normal standby[ 0.712982] print_constraints: VDVI: 1800 mV normal standby[ 0.719543] print_constraints: VSIM: 1800 <--> 3000 mV at 1800 mV normal standby[ 0.721710] omap_i2c omap_i2c.3: bus 3 rev1.3.12 at 100 kHz[ 0.748443] Switching to clocksource 32k_counter[ 1.068511] NET: Registered protocol family 2[ 1.071014] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)[ 1.075744] TCP established hash table entries: 8192 (order: 4, 65536 bytes)[ 1.076385] TCP bind hash table entries: 8192 (order: 6, 294912 bytes)[ 1.082031] TCP: Hash tables configured (established 8192 bind 8192)[ 1.082305] TCP reno registered[ 1.082397] UDP hash table entries: 128 (order: 1, 10240 bytes)[ 1.082885] UDP-Lite hash table entries: 128 (order: 1, 10240 bytes)[ 1.084716] NET: Registered protocol family 1[ 1.088470] RPC: Registered named UNIX socket transport module.[ 1.088531] RPC: Registered udp transport module.[ 1.088562] RPC: Registered tcp transport module.[ 1.088592] RPC: Registered tcp NFSv4.1 backchannel transport module.[ 1.091033] NetWinder Floating Point Emulator V0.97 (double precision)[ 1.315063] VFS: Disk quotas dquot_6.5.2[ 1.315673] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)[ 1.322937] JFFS2 version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc.[ 1.325744] msgmni has been set to 481[ 1.336486] io scheduler noop registered[ 1.336547] io scheduler deadline registered[ 1.337127] io scheduler cfq registered (default)[ 1.343963] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled[ 1.362609] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0[ 1.368164] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1[ 1.371826] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2[ 2.026977] console [ttyO2] enabled[ 2.131408] brd: module loaded[ 2.190582] loop: module loaded[ 2.216552] mtdoops: mtd device (mtddev=name/number) must be supplied[ 2.224914] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-bit)[ 2.236785] Creating 5 MTD partitions on "omap2-nand.0":[ 2.242828] 0x000000000000-0x000000080000 : "X-Loader"[ 2.266632] 0x000000080000-0x000000260000 : "U-Boot"[ 2.285125] 0x000000260000-0x000000280000 : "U-Boot Env"[ 2.303131] 0x000000280000-0x000000680000 : "Kernel"[ 2.323364] 0x000000680000-0x000010000000 : "File System"[ 2.463623] OneNAND driver initializing[ 2.491027] usbcore: registered new interface driver asix[ 2.498931] usbcore: registered new interface driver cdc_ether[ 2.507629] usbcore: registered new interface driver net1080[ 2.515655] usbcore: registered new interface driver cdc_subset[ 2.523864] usbcore: registered new interface driver zaurus[ 2.531799] usbcore: registered new interface driver cdc_ncm[ 2.544219] usbcore: registered new interface driver cdc_wdm[ 2.550506] Initializing USB Mass Storage driver...[ 2.557617] usbcore: registered new interface driver usb-storage[ 2.564392] USB Mass Storage support registered.[ 2.572601] usbcore: registered new interface driver libusual[ 2.580871] usbcore: registered new interface driver usbtest[ 2.591735] mousedev: PS/2 mouse device common for all mice[ 2.613464] input: twl4030_pwrbutton as /devices/platform/omap/omap_i2c.1/i2c-1/1-0049/twl4030_pwrbutton/input/input0[ 2.639373] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0[ 2.649749] i2c /dev entries driver[ 2.661437] Driver for 1-wire Dallas network protocol.[ 2.676208] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec[ 2.685394] twl4030_wdt twl4030_wdt: Failed to register misc device[ 2.692810] twl4030_wdt: probe of twl4030_wdt failed with error -16[ 2.949523] usbcore: registered new interface driver usbhid[ 2.955718] usbhid: USB HID core driver[ 2.959808] oprofile: hardware counters not available[ 2.965332] oprofile: using timer interrupt.[ 2.971435] TCP cubic registered[ 2.974884] Initializing XFRM netlink socket[ 2.980072] NET: Registered protocol family 17[ 2.985229] NET: Registered protocol family 15[ 2.990753] Registering the dns_resolver key type[ 2.997711] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1[ 3.007812] ThumbEE CPU extension supported.[ 3.121765] clock: disabling unused clocks to save power[ 3.137634] regulator_init_complete: VDVI: incomplete constraints, leaving on[ 3.145843] regulator_init_complete: VDAC: incomplete constraints, leaving on[ 3.158935] input: gpio-keys as /devices/platform/gpio-keys/input/input1[ 3.173675] twl_rtc twl_rtc: setting system clock to 2009-01-16 13:50:05 UTC (1232113805)[ 3.199829] CLEANMARKER node found at 0x00000000 has totlen 0xc != normal 0x0[ 3.230072] CLEANMARKER node found at 0x00020000 has totlen 0xc != normal 0x0[ 3.256439] CLEANMARKER node found at 0x00040000 has totlen 0xc != normal 0x0[ 3.283721] CLEANMARKER node found at 0x00060000 has totlen 0xc != normal 0x0[ 3.312866] CLEANMARKER node found at 0x00080000 has totlen 0xc != normal 0x0[ 3.338989] CLEANMARKER node found at 0x000a0000 has totlen 0xc != normal 0x0[ 3.365570] CLEANMARKER node found at 0x000c0000 has totlen 0xc != normal 0x0[ 3.395812] CLEANMARKER node found at 0x000e0000 has totlen 0xc != normal 0x0[ 3.422821] CLEANMARKER node found at 0x00100000 has totlen 0xc != normal 0x0[ 3.447937] mmc0: new high speed SD card at address 0002[ 3.460937] mmcblk0: mmc0:0002 00000 971 MiB (ro)[ 3.469726] CLEANMARKER node found at 0x00120000 has totlen 0xc != normal 0x0[ 3.506652] CLEANMARKER node found at 0x00140000 has totlen 0xc != normal 0x0[ 3.514495] mmcblk0: p1 p2[ 3.547515] CLEANMARKER node found at 0x00160000 has totlen 0xc != normal 0x0[ 3.573699] CLEANMARKER node found at 0x00180000 has totlen 0xc != normal 0x0[ 3.599487] CLEANMARKER node found at 0x001a0000 has totlen 0xc != normal 0x0[ 3.624908] CLEANMARKER node found at 0x001c0000 has totlen 0xc != normal 0x0[ 3.651550] CLEANMARKER node found at 0x001e0000 has totlen 0xc != normal 0x0[ 3.676696] CLEANMARKER node found at 0x00200000 has totlen 0xc != normal 0x0[ 3.702117] CLEANMARKER node found at 0x00220000 has totlen 0xc != normal 0x0[ 3.727996] CLEANMARKER node found at 0x00240000 has totlen 0xc != normal 0x0[ 3.753265] CLEANMARKER node found at 0x00260000 has totlen 0xc != normal 0x0[ 3.778869] CLEANMARKER node found at 0x00280000 has totlen 0xc != normal 0x0[ 3.804382] CLEANMARKER node found at 0x002a0000 has totlen 0xc != normal 0x0[ 3.829864] CLEANMARKER node found at 0x002c0000 has totlen 0xc != normal 0x0[ 3.855102] CLEANMARKER node found at 0x002e0000 has totlen 0xc != normal 0x0[ 3.880615] CLEANMARKER node found at 0x00300000 has totlen 0xc != normal 0x0[ 3.906005] CLEANMARKER node found at 0x00320000 has totlen 0xc != normal 0x0[ 3.931457] CLEANMARKER node found at 0x00340000 has totlen 0xc != normal 0x0[ 3.956573] CLEANMARKER node found at 0x00360000 has totlen 0xc != normal 0x0[ 3.981964] CLEANMARKER node found at 0x00380000 has totlen 0xc != normal 0x0[ 4.007598] CLEANMARKER node found at 0x003a0000 has totlen 0xc != normal 0x0[ 4.032897] CLEANMARKER node found at 0x003c0000 has totlen 0xc != normal 0x0[ 4.058441] CLEANMARKER node found at 0x003e0000 has totlen 0xc != normal 0x0[ 4.083801] CLEANMARKER node found at 0x00400000 has totlen 0xc != normal 0x0[ 4.109100] CLEANMARKER node found at 0x00420000 has totlen 0xc != normal 0x0[ 4.134674] CLEANMARKER node found at 0x00440000 has totlen 0xc != normal 0x0[ 4.160003] CLEANMARKER node found at 0x00460000 has totlen 0xc != normal 0x0[ 4.185485] CLEANMARKER node found at 0x00480000 has totlen 0xc != normal 0x0[ 4.210906] CLEANMARKER node found at 0x004a0000 has totlen 0xc != normal 0x0[ 4.240234] CLEANMARKER node found at 0x004c0000 has totlen 0xc != normal 0x0[ 4.270965] CLEANMARKER node found at 0x004e0000 has totlen 0xc != normal 0x0[ 4.297271] CLEANMARKER node found at 0x00500000 has totlen 0xc != normal 0x0[ 4.322906] CLEANMARKER node found at 0x00520000 has totlen 0xc != normal 0x0[ 4.348663] CLEANMARKER node found at 0x00540000 has totlen 0xc != normal 0x0[ 4.374084] CLEANMARKER node found at 0x00560000 has totlen 0xc != normal 0x0[ 4.399902] CLEANMARKER node found at 0x00580000 has totlen 0xc != normal 0x0[ 4.425445] CLEANMARKER node found at 0x005a0000 has totlen 0xc != normal 0x0[ 4.451568] CLEANMARKER node found at 0x005c0000 has totlen 0xc != normal 0x0[ 4.477661] CLEANMARKER node found at 0x005e0000 has totlen 0xc != normal 0x0[ 4.503692] CLEANMARKER node found at 0x00600000 has totlen 0xc != normal 0x0[ 4.529113] CLEANMARKER node found at 0x00620000 has totlen 0xc != normal 0x0[ 4.554931] CLEANMARKER node found at 0x00640000 has totlen 0xc != normal 0x0[ 4.580718] CLEANMARKER node found at 0x00660000 has totlen 0xc != normal 0x0[ 4.606903] CLEANMARKER node found at 0x00680000 has totlen 0xc != normal 0x0[ 4.633392] CLEANMARKER node found at 0x006a0000 has totlen 0xc != normal 0x0[ 4.659912] CLEANMARKER node found at 0x006c0000 has totlen 0xc != normal 0x0[ 4.687347] CLEANMARKER node found at 0x006e0000 has totlen 0xc != normal 0x0[ 4.713012] CLEANMARKER node found at 0x00700000 has totlen 0xc != normal 0x0[ 4.739135] CLEANMARKER node found at 0x00720000 has totlen 0xc != normal 0x0[ 4.765502] CLEANMARKER node found at 0x00740000 has totlen 0xc != normal 0x0[ 4.791381] CLEANMARKER node found at 0x00760000 has totlen 0xc != normal 0x0[ 4.817352] CLEANMARKER node found at 0x00780000 has totlen 0xc != normal 0x0[ 4.843627] CLEANMARKER node found at 0x007a0000 has totlen 0xc != normal 0x0[ 4.877136] CLEANMARKER node found at 0x007c0000 has totlen 0xc != normal 0x0[ 4.903198] CLEANMARKER node found at 0x007e0000 has totlen 0xc != normal 0x0[ 4.932769] CLEANMARKER node found at 0x00800000 has totlen 0xc != normal 0x0[ 4.958679] CLEANMARKER node found at 0x00820000 has totlen 0xc != normal 0x0[ 4.985351] CLEANMARKER node found at 0x00840000 has totlen 0xc != normal 0x0[ 5.012054] CLEANMARKER node found at 0x00860000 has totlen 0xc != normal 0x0[ 5.037689] CLEANMARKER node found at 0x00880000 has totlen 0xc != normal 0x0[ 5.063873] CLEANMARKER node found at 0x008a0000 has totlen 0xc != normal 0x0[ 5.090545] CLEANMARKER node found at 0x008c0000 has totlen 0xc != normal 0x0[ 5.117462] CLEANMARKER node found at 0x008e0000 has totlen 0xc != normal 0x0[ 5.143035] CLEANMARKER node found at 0x00900000 has totlen 0xc != normal 0x0[ 5.169647] CLEANMARKER node found at 0x00920000 has totlen 0xc != normal 0x0[ 5.196166] CLEANMARKER node found at 0x00940000 has totlen 0xc != normal 0x0[ 5.223785] CLEANMARKER node found at 0x00960000 has totlen 0xc != normal 0x0[ 5.250579] CLEANMARKER node found at 0x00980000 has totlen 0xc != normal 0x0[ 5.277923] CLEANMARKER node found at 0x009a0000 has totlen 0xc != normal 0x0[ 5.303558] CLEANMARKER node found at 0x009c0000 has totlen 0xc != normal 0x0[ 5.329315] CLEANMARKER node found at 0x009e0000 has totlen 0xc != normal 0x0[ 5.355102] CLEANMARKER node found at 0x00a00000 has totlen 0xc != normal 0x0[ 5.380859] CLEANMARKER node found at 0x00a20000 has totlen 0xc != normal 0x0[ 5.407226] CLEANMARKER node found at 0x00a40000 has totlen 0xc != normal 0x0[ 5.433105] CLEANMARKER node found at 0x00a60000 has totlen 0xc != normal 0x0[ 5.458770] CLEANMARKER node found at 0x00a80000 has totlen 0xc != normal 0x0[ 5.484619] CLEANMARKER node found at 0x00aa0000 has totlen 0xc != normal 0x0[ 5.510345] CLEANMARKER node found at 0x00ac0000 has totlen 0xc != normal 0x0[ 5.535919] CLEANMARKER node found at 0x00ae0000 has totlen 0xc != normal 0x0[ 5.561676] CLEANMARKER node found at 0x00b00000 has totlen 0xc != normal 0x0[ 5.587799] CLEANMARKER node found at 0x00b20000 has totlen 0xc != normal 0x0[ 5.613555] CLEANMARKER node found at 0x00b40000 has totlen 0xc != normal 0x0[ 5.639190] CLEANMARKER node found at 0x00b60000 has totlen 0xc != normal 0x0[ 5.665466] CLEANMARKER node found at 0x00b80000 has totlen 0xc != normal 0x0[ 5.691131] CLEANMARKER node found at 0x00ba0000 has totlen 0xc != normal 0x0[ 5.716918] CLEANMARKER node found at 0x00bc0000 has totlen 0xc != normal 0x0[ 5.742950] CLEANMARKER node found at 0x00be0000 has totlen 0xc != normal 0x0[ 5.769165] CLEANMARKER node found at 0x00c00000 has totlen 0xc != normal 0x0[ 5.795257] CLEANMARKER node found at 0x00c20000 has totlen 0xc != normal 0x0[ 5.821441] CLEANMARKER node found at 0x00c40000 has totlen 0xc != normal 0x0[ 5.847717] CLEANMARKER node found at 0x00c60000 has totlen 0xc != normal 0x0[ 5.873748] CLEANMARKER node found at 0x00c80000 has totlen 0xc != normal 0x0[ 5.900268] CLEANMARKER node found at 0x00ca0000 has totlen 0xc != normal 0x0[ 5.928436] CLEANMARKER node found at 0x00cc0000 has totlen 0xc != normal 0x0[ 5.955932] CLEANMARKER node found at 0x00ce0000 has totlen 0xc != normal 0x0[ 5.981933] CLEANMARKER node found at 0x00d00000 has totlen 0xc != normal 0x0[ 6.007995] CLEANMARKER node found at 0x00d20000 has totlen 0xc != normal 0x0[ 6.034576] CLEANMARKER node found at 0x00d40000 has totlen 0xc != normal 0x0[ 6.060638] CLEANMARKER node found at 0x00d60000 has totlen 0xc != normal 0x0[ 6.086517] CLEANMARKER node found at 0x00d80000 has totlen 0xc != normal 0x0[ 6.112396] CLEANMARKER node found at 0x00da0000 has totlen 0xc != normal 0x0[ 6.138458] CLEANMARKER node found at 0x00dc0000 has totlen 0xc != normal 0x0[ 6.164886] CLEANMARKER node found at 0x00de0000 has totlen 0xc != normal 0x0[ 6.191040] CLEANMARKER node found at 0x00e00000 has totlen 0xc != normal 0x0[ 6.216583] CLEANMARKER node found at 0x00e20000 has totlen 0xc != normal 0x0[ 6.243011] CLEANMARKER node found at 0x00e40000 has totlen 0xc != normal 0x0[ 6.268798] CLEANMARKER node found at 0x00e60000 has totlen 0xc != normal 0x0[ 6.294525] CLEANMARKER node found at 0x00e80000 has totlen 0xc != normal 0x0[ 6.320800] CLEANMARKER node found at 0x00ea0000 has totlen 0xc != normal 0x0[ 6.348541] CLEANMARKER node found at 0x00ec0000 has totlen 0xc != normal 0x0[ 6.378112] CLEANMARKER node found at 0x00ee0000 has totlen 0xc != normal 0x0[ 6.407989] CLEANMARKER node found at 0x00f00000 has totlen 0xc != normal 0x0[ 6.443145] CLEANMARKER node found at 0x00f20000 has totlen 0xc != normal 0x0[ 6.482971] CLEANMARKER node found at 0x00f40000 has totlen 0xc != normal 0x0[ 6.521179] CLEANMARKER node found at 0x00f60000 has totlen 0xc != normal 0x0[ 6.557739] CLEANMARKER node found at 0x00f80000 has totlen 0xc != normal 0x0[ 6.591674] CLEANMARKER node found at 0x00fa0000 has totlen 0xc != normal 0x0[ 6.628540] CLEANMARKER node found at 0x00fc0000 has totlen 0xc != normal 0x0[ 6.667144] CLEANMARKER node found at 0x00fe0000 has totlen 0xc != normal 0x0[ 6.700317] CLEANMARKER node found at 0x01000000 has totlen 0xc != normal 0x0[ 6.737335] CLEANMARKER node found at 0x01020000 has totlen 0xc != normal 0x0[ 6.779144] CLEANMARKER node found at 0x01040000 has totlen 0xc != normal 0x0[ 6.818817] CLEANMARKER node found at 0x01060000 has totlen 0xc != normal 0x0[ 8.402801] JFFS2 notice: (1) jffs2_build_xattr_subsystem: complete building xattr subsystem, 0 of xdatum (0 uncheck.[ 8.428680] VFS: Mounted root (jffs2 filesystem) on device 31:4.[ 8.436340] Freeing init memory: 308KFailed to open /dev/kmsg for logging: No such file or directory
Can you try compiling the kernel with the option CONFIG_DEVTMPFS_MOUNT=y enabled?
-Renjith | www.pathpartnertech.com | Verify the answer if you think your query is resolved