I am following the instructions on the wiki page, but it does not configure correctly.
#./configure --host=arm-linux --prefix=$HOME/install CC=arm-none-linux-gnueabi-gcc CXX=arm-none-linux-gnueabi-g++
configure: WARNING: If you wanted to set the --build type, don't use --host.
If a cross compiler is detected then cross compile mode will be used.
checking for a BSD-compatible install... /usr/bin/install -c
checking whether build environment is sane... yes
checking for gawk... gawk
checking whether make sets $(MAKE)... yes
checking for arm-linux-strip... no
checking for strip... strip
checking for C++ compiler default output file name... configure: error: C++ compiler cannot create executables
See `config.log' for more details.
Has anyone been able to get this tool to configure correctly?