Hi,
1) We are using twl4030 bci feature for charging
2) We are using the linux driver that exists in open source
3) We find that twl4030battery_interrupt which is for battery insertion/removal keeps getting
called, shouldn't it be called only during insertion or removal only
4) If i have a battery permanently connected, can this interrupt be disabled?
5) How is battery protected from overcharging?
6) This driver enables/disables only AC/USB charging - Is charging done automatically?
Battery driver:
http://git.omapzoom.com/?p=kernel/omap.git;a=commit;h=32f86140cddc1ef198fb1f642ee1f56ab409e1bd