Hello,
I have a problem: I asked many times about the same framebuffer going
to LCD port and PAL and I have different answers.
In Figure 15-70 of spruf98b.pdf I see the Graphics Path. I'm sorry I
ask again if I can select this (G) in both Overlay Managers.
Regarding Documentation/arm/OMAP/DSS it seems to be possible in
omap3503 and obviously in omap3530.
I'm really sorry but I can't understand why I get a different answer from TI.
Example: I write a graphic menu to a frame buffer and I'd like to see
it in 720p from LCD port and also scaled down to PAL from Video port.
TI told me that (G) can go to only one Overlay Manager.
So I can suppose that TI has this limitation with 2.6.22 official
kernel, but I think that if I start the project today with omap3503 now I
don't have this problem, because I'll use at least linux-omap-2.6.28,
or the mainline kernel, if it will be completed in about six months.