Our SD Card write function is slow: 2 ms to 22 ms. A related problem may be that BADA errors (on MMCHS_STAT) are reported on every write to MMCHS_DATA. This does doesn't make sense because BWE=1 on MMCHS_PSTATE before the write.
Even though these errors are generated, the data is successfully written to the SD card. However, it takes 2 ms to 22 ms to get TC (trasnfer complete).
MMCHS_BLK BLEN is set to 0x200 (512).