Hi,
I have a question about am3517 ecc. The psp I used is 04.02.00.07, the command nandecc is as below:
# nandecc [ hw <hw_type> | sw | bch4_sw | bch8_sw ]
Usage:
sw - Set software ECC for NAND
hw <hw_type> - Set hardware ECC for NAND
<hw_type> - 1 for Kernel/FileSystem ECC layout
2 for X-loader/U-boot ECC layout
bch4_sw - Set 4-bit BCH ECC for NAND
bch8_sw - Set 8-bit BCH ECC for NAND
Does this mean that sw, bch4_sw and bch8_sw are useless just because what I need to write in nand are x-loader, uboot, kernel and filesystem?