Hi,
Could somebody tell me the differences between am3517-linux-psp-04.02.00.07 and am3517-linux-psp-03.00.00.05, especially about NAND driver in uboot?
What I know is that: am3517-linux-psp-03.00.00.05 uses 'nandecc sw/hw', I need to use 'nandecc sw' to flash u-boot; am3517-linux-psp-04.02.00.07 uses 'nandecc sw/hw 2/hw 1/bch4_sw/bch8_sw', I could use 'nandecc hw 2' to flash u-boot. Is there any bug in NAND driver of am3517-linux-psp-03.00.00.05? Is 'nandecc hw 2' better than 'nandecc sw' when flashing u-boot?