I'm trying to enable SSC (Spread Spectrum Clocking) feature for DM3730 Processor to reduce the EMI from our LCD and camera modules. I write modulation frequency and DeltaMStep values ( 0xFECDC09 - for 1% variation; calculated as per the TRM) in CONTROL_PER_DPLL_SPREADING_FREQ and enbling it by writing 0x10 in the CONTROL_PER_DPLL_SPREADING register. When I probe the LCD PCLK I did see some spreading. But it is not consistant. When I entered the values today I didn't see any change. Please give me any suggestions.
Thanks in advance,
Prathap