I am having trouble bringing up a Mistral AM/DM37X EVM (rev g) board using some of the samples I've found. I have installed CCS 6.x, and DSP/BIOS. I would like to run a test application that runs a simple FFT on the DSP and displays the results via printf over one of the UARTS. This should validate the two things that I need to do, run an application on the ARM Cortex and use the DSP for the performance gain necessary to complete the FFTs.
I am able to build and run over the TI XDS200 USB debug probe, the clock_OMAP3530_CortexA project. If I comment out the call to Bios_exit(), it will run forever, but I do not see any data on the UART as a result of the printf statements.
I am able to build but not run any of the DSPLIB projects that I have attempted. I have tried a few of the fft samples. Each of which reports that "the device functional clock appears to be off ... " I found some other posts reporting this problem, but I have not yet understood the response to the point where I can take corrective measures. Does a sample project exist for this board that can help with this problem?