• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » OMAP™ Processors » All Tags » 138
Share
OMAP™ Processors
  • Forums
  • Announcements

Browse by Tags

OMAP™ Processors

Welcome to the OMAP™ Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
138
  • "OMAP-L138 LCDK"
  • _c_int00 runtime supervisor L138 ARM9 peripheral
  • 03.22.00.03
  • 138 Nand Flash U-Boot
  • 16bit NAND
  • 2.6.29
  • 2.6.37
  • 512MB
  • 6748
  • 6748 DSP OMAP-L138 CCS4.2
  • 6748 OMAP-L138
  • 6748 TMS320C6748 LCDK
  • 674x
  • altium OMAP L138 LCDK orcad 16.2 tmdxlcdk138
  • AM1705 OMAP-L137
  • am1802 McASP
  • AM18xx
  • BT.1120
  • hang
  • l138
  • OMAP
  • OMAPl138
  • OMAP-L138
  • spi0
  • vpif
Related Posts
  • Forum Post: VPIF, HD video input

    Mohammad Ali Koteich Mohammad Ali Koteich
    Hi, How is it possible to utilize the VPIF port for input from a standard HD cam?.. (BT.1120 output from cam seems to be rare) Are there any HDMI to VPIF converters out there? I tried searching.. Found SiL9135, but it's overkill (audio, 2xHDMI, 144 pins, 20x20mm).. Furthermore, since...
    on Apr 3, 2012
  • Forum Post: RE: McASP on OMAP-L138

    Boris Ruvinsky Boris Ruvinsky
    Hi Bobby. Thank you very much for your respond and help. I was always thinking that #1 was a typo, thank you for clarifying that. Is there any timing available for AHCLKX/R to ACLKX/R when AHCLKX/R (external) are used to generate ACLKX/R? There should be some timing for that but I can't find...
    on May 8, 2012
  • Forum Post: Omap L138 who prints "OMAP-L138 initialization passed"

    tom campbell tom campbell
    We have a custom OMAP L-138 board with a revision 2.0 silicon chip. The board doesn't boot reliably from power on. It prints some or all of "OMAP-L138 initialization passed" and dies. It works reliably from the reset button. We are working on the theory that it is caused by the Silicon...
    on May 14, 2012
  • Forum Post: mDDR/DDR2

    hadded franck hadded franck
    Hello, I use the CCS V5 to check my hardware for the following configuration: - OMAP_l138 => DSP/ARM 300Mhz:mDDR/DDR2 150Mhz - DDR2 -667D => 16-bit DDR2 with up to 512-MB memory address space (64Mb X16 X8 Banks ) -FLASH NOR SPI -NAND FLASH DDR2 Configuration Register Parameter: -SDCFG...
    on Jun 18, 2012
  • Forum Post: Sample applications not working on omapL138-hawkboard

    Kiran Kumar Kiran Kumar
    Dear All, I am new to OMAP SOC and I wanted to start experiments on the Hawkboard. However I am stuck at a point where I am not able to run the sample applications provided by DVSDK. When I try to run the pre-compiled application I see the below error. I am trying to understand where to start to...
    on Jun 27, 2012
  • Forum Post: RE: OMAP L138 EMIF for 1bit ECC non-CE NAND

    Pankaj katiyar Pankaj katiyar
    Any one??? I am having trouble booting up with 1bit ECC NAND. The only option available is to respin the board with 4-bit ECC. Also OMAP RBL configures 5 registers CE2CFG, CE3CFG,CE4CFG,CE5CFG,NANDFCR. If i read the default value which is after reset, I can see that EMIFA is configured for 4-bit...
    on Jul 11, 2012
  • Forum Post: ECAP1 Input Voltage Range Of AM1808

    Zeng_wg Zeng_wg
    Dears: I will use ECAP1 to capture a analog signal's fall edge, But I don't find the input voltage range of this pin. Does it 0 to 3.3V??
    on Jul 15, 2012
  • Forum Post: waiting for SFT on OMAP-L138... command failed

    feng lin feng lin
    Hi, I am trying to erase nand flash using commands "sfh_omap_l38.exe -erase -flashType NAND" on the omap-l138 board. The information output is as follows: If there is some problem with the nand flash ?Even the nand flash is not working. thank you Regards
    on Aug 21, 2012
  • Forum Post: error in ethernet connection

    Michelle Lopez Michelle Lopez
    I am using evmomaqpl138, spectrum digital sd560v2 and starterware 01.10.03.03 ethernet examples. I have a switch where I have connected the network, and a hub where I have connected the evm and the host pc. I am trying to get the ipaddress in the code using a static ip address, staitc gateway and static...
    on Sep 5, 2012
  • Forum Post: AM1808 Mini USB support in PC

    francis kumar francis kumar
    Hi All, I am using AM1808 Processor. While connecting the mini USB to Windows XP PC, It has detected as Hardware found. It is detected in PC as “Linux File-CD Gadget” act as a device. What could be the region. I need to install any supported files to XP PC. My USB A is working...
    on Sep 7, 2012
  • Forum Post: ARM9_0: Can't Run Target CPU

    Michelle Lopez Michelle Lopez
    Hello all, I have been trying to run the IPC example found in StarterWare for the OmapL138 but am encountering problems. I was able to load both binaries into the ARM and the DSP and was able to group the cores. I have a problem when I try to run the cores grouped. First i got a message that it was...
    on Sep 17, 2012
  • Forum Post: EDMA3_LLD_02_11_05_02

    Steven Sharp Nelson Steven Sharp Nelson
    where to download the EDMA3_LLD_02_11_05_02 or the last release of EDMA3?
    on Nov 12, 2012
  • Forum Post: edma3_lld_02_11_06_01;

    Steven Sharp Nelson Steven Sharp Nelson
    when i build those source of edma3_lld_02_11_06_01; I find these errors,what should i do ?,The symbol of DVTEvent_Log and LOG_printf4 are come from edma3_log.h,I my mind the symbol of LOG_printf4 are BIOS5's founction. how to solve this?
    on Nov 13, 2012
  • Forum Post: RE: edma3_lld_02_11_06_01;

    Steven Sharp Nelson Steven Sharp Nelson
    I try it,that can be build success. also i can delete all the part contain these macros . but if i need these logs ,what can i do to solve these incompatible problem?
    on Nov 13, 2012
  • Forum Post: OMAPL138 frequency setting

    allen chen96638 allen chen96638
    Hi all, I have a question on the CPU frequency。 My board power supply chip is TPS65070 , just like the logicpd design, and now processor work frequency is 300M. But now I want to increase the frequency to 475M, how should I do? (just ONLY need to rewrite the PLL0 configuration? ) The PDF saids that...
    on Jan 6, 2013
  • Forum Post: AM1802 SPI boot problem

    Z-SEED Z-SEED
    Hi, I have a AM1802 target board using SPI1 FLASH boot. I have set the boot mode pins as SPI1 FLASH mode, and the board was used to be booted successfully. Then I measured the SPI pins, OSCIN, OSCOUT, and boot mode pins using oscilloscope. At last, I powered down the target board. When I powered up...
    on Feb 1, 2013
  • Forum Post: RE: AM1808 Flash User Guide

    francis kumar francis kumar
    Hi, I am working on AM1808 processor, I used NAND flash in our design which is micron 2Gb part:MT29F2G08ABAEAWP-IT:E TR Also i am using SPI flash in my design. I would like to use NAND flash for only my root filesystem. Can i have steps how to convert Filesys in to JFFS2 and how it can be done in...
    on Apr 20, 2013
  • Forum Post: L138: SPI0 CS4 hanging during linux probe

    Scott Battocchi Scott Battocchi
    Hi, We have a system using the LogicPD SOM on our own baseboard running Linux (no dsp application at the moment, though we do plan to use the dsplink module in the future). There are three NXP SC16IS762 SPI to dual UART chips (linux driver merged in sc16is7x2) on SPI0 CS2, CS3, CS4. We have the system...
    on May 9, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use