• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » OMAP™ Processors » All Tags » OMAPL137
Share
OMAP™ Processors
  • Forums
  • Announcements

Browse by Tags

OMAP™ Processors

Welcome to the OMAP™ Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
OMAPL137
  • AM1808
  • boot
  • C6747
  • C674x
  • Codec Engine
  • DSP
  • DSP/BIOS
  • DSP/BIOS Link
  • dsplink
  • EDMA
  • L137
  • l138
  • L-138
  • Linux
  • McASP
  • NAND
  • OMAP
  • omap l137
  • OMAP L-137
  • omap l138
  • OMAP L-138
  • OMAP_L138
  • OMAP-L137
  • OMAPl138
  • OMAP-L138
Related Posts
  • Forum Post: EDMA to SPI - No Activity

    nkeddem nkeddem
    I am attempting to ulitize the EDMA to loop out data that I have in a 1d array on a OMAPL137. I am getting no activity on the SPI line when I execute my program but if i manually change the data found in SPIDAT1 I get line activity. It is almost as if I am missing something in my EDMA configuration but...
    on Apr 16, 2009
  • Forum Post: DSP DMA on OMAP-L137

    Flamingo Flamingo
    I'm using MV Linux on the ARM9 and DSP/BIOS on the DSP side of the OMAP-L137. I need to DMA from the SPI1 to memory on the DSP side. (MV Linux will not be able to keep up with the real-time control requirements.) The number of 16-bit transfers is variable from one transfer to the next, and the...
    on May 11, 2009
  • Forum Post: Re: RTSC Wizard, Codec Engine

    Flamingo Flamingo
    Thanks. Using this info I found nm6x. However, when I entered its location into RTSC, the following two screens were the same. That is, on step 5 of 6, I get two tables: one with blank Config Name and another with blank Return values. I don't know if I need to put anything in there. I hit the Next...
    on May 12, 2009
  • Forum Post: fast SRAM, OMAP-L137

    Flamingo Flamingo
    One of my hardware engineers asks: "We are having variable success getting SRAM. The 166MHz ISSI part seems to be unobtainable right now. There is a 140MHZ ISSI part with some lead time. There is a 133MHZ Micron part that is available. I know if I plug into my PC any speed of RAM the bios...
    on May 12, 2009
  • Forum Post: Re: Can omap-l137 connect a lcd with touch screen?

    Haroldo Haroldo
    Hi Mariana By chance do you have any idea of where I could acquire the DSKDA830 User Interface Board, I already called SpectrumDigital but they said the only way to get it is thru TI and you can only buy it as a whole kit. I have already purchased the OMAP-L137 EVM so I´m not interested in...
    on May 19, 2009
  • Forum Post: Re: Can omap-l137 connect a lcd with touch screen?

    Haroldo Haroldo
    Hi Mariana, Thanks for the update, but do you know if TI plans to sell it separetely?
    on May 19, 2009
  • Forum Post: [OMAPL137] SIO stacked device

    Flamingo Flamingo
    I'm using the OMAP-L137. SPI 1 will be connected to an ADS8330 ADC. Commands to drive the ADS8330 will be output via SPI 1. nCONVST will be a GPIO pin from the OMAP-L137. Additional setup and control associated with the ADC will be via 6 GPIO pins. One of these will be a GPIO input, probably an...
    on May 20, 2009
  • Forum Post: IUNIVERSAL derived makefile

    Flamingo Flamingo
    I am developing an IUNIVERSAL-derived codec for the OMAP-L137. Using CCS, I've developed a library project for the codec and a separate project for main and some background tasks. Both build. Now I'd like to test them. {For test purposes, the library and tasks just turn on some test LEDs right...
    on Jun 1, 2009
  • Forum Post: Re: IUNIVERSAL derived makefile

    Flamingo Flamingo
    My correspondance with my TI rep suggests that you and he disagree on this: "When Engine is opened, the dsp image gets loaded and the DSP starts running. The Codec Engine remote server running on DSP waits for the ARM to instantiate a codec instance using _create(). You may however, create static...
    on Jun 2, 2009
  • Forum Post: Connecting Lauterbach JTAG probe to OMAP-L137 EVM

    BryceG BryceG
    Hello support, I am trying to connect a Lauterbach probe to the 20 pin JTAG on the OMAP-L137 EVM, and not having much luck. Is there any documentation describing how to do this? I am using the 4/15 update to the Trace32 software. When I connect the probe to the target, I get a "running (power...
    on Jun 2, 2009
  • Forum Post: Re: IUNIVERSAL derived makefile

    Flamingo Flamingo
    I had been using a Rules.make derived from other TI packages, but none of them looked like yours, so I re-did that. It didn't help, but I finally got XDCPATH defined in a way in the Makefile that worked. So, I have successfully run "make genpackage, "make", and "make genserver"...
    on Jun 4, 2009
  • Forum Post: Documentation for programming the TIMERS on the OMAP-L137

    BryceG BryceG
    I am looking for the documentation that describes how to program the timers on the OMAP-L137. I have omap-l137.pdf which describes that there is 1 64 bit timer (or 2 32 bit timers), lists the registers, but does not describe how to use the timers or program the timer clock. I have also looked at sprug84b...
    on Jun 16, 2009
  • Forum Post: [OMAPL137] dsplinkk.ko

    Flamingo Flamingo
    I'm using the OMAP-L137. I'm developing a codec. I have purchased the license for MontaVista Linux. My target is custom (not the eval board). I have rebuilt dsplink. Associated with that rebuild, six copies of dsplinkk.ko were created: 1. gpp/BUILD/EXPORT/RELEASE 2. gppBUILDPMGR/BIN...
    on Jul 3, 2009
  • Forum Post: Failed to open (codec engine)

    Flamingo Flamingo
    OMAP-L137, custom codec, custom hardware, custom Linux, custom dsplink. I've rebuilt Linux, cmemk.ko, dsplinkk.ko, and now I'm trying to run my app. See "Oops" below. (Memory_alloc fails when dereferencing a null pointer at 0x0000000a.) Any hints? I've not yet been able to connect...
    on Jul 8, 2009
  • Forum Post: [OMAPL137] SDRAM, Codec Engine

    Flamingo Flamingo
    Each time I add more GT_ trace calls in my app, the trace messages from Engine_open seem to suggest that the code is making it further without error. Since I'm not making any other changes, this screams of memory partitioning, stack, heap, etc errors. My target board has twice the SDRAM as...
    on Jul 8, 2009
  • Forum Post: [OMAPL137] Memory_contigAlloc failure

    Flamingo Flamingo
    I'm trying to debug some of my code. I have dsplink built with debug. I think I have cmem built with debug (although I don't see all the messages that I'm expecting, so that may not work the way I think it does.) CE_DEBUG=2. As you can see in the output below, I see failures in cmemk....
    on Jul 27, 2009
  • Forum Post: Debugging Engine_open

    Flamingo Flamingo
    My Engine_open hangs in SEM_pend: backtrace = #0 0x40031fe4 in __new_sem_wait (sem=0x4e1d8) at ../nptl/sysdeps/unix/sysv/linux/sem_wait.c:48 #1 0x00018c58 in Sem_pend () #2 0x00012ed4 in doCmd () #3 0x000143b4 in Processor_create () #4 0x00010710 in Engine_open () #5 0x0000a284 in smain (argc...
    on Jul 30, 2009
  • Forum Post: [OMAPL137] lad, codec engine, dsplink

    Flamingo Flamingo
    I'm currently using a reconfigured dsplink-1_61 (expanding the code/data space, using memory from 0xc2000000 for DDR2 and memory above that for cmem (c3000000 - c4e00000), with the following in the config/all file. /** ==========================================================================...
    on Jul 30, 2009
  • Forum Post: GT_trace and engineering notation

    Flamingo Flamingo
    I am using GT_trace calls to debug some parameter passing problems between the app and server sides of my codec. When I use %e on the app side, I see the numbers. When I use %e on the DSP-server side, I see "e". Is there a engineering notation format that has been implemented on the DSP side...
    on Aug 3, 2009
  • Forum Post: [OMAPL137] SEM basics

    Flamingo Flamingo
    I have a DSP-server codec running along with 2 background tasks. One day, I'm hoping to have a GPIO-driven interrupt that posts the semaphore that I discuss below. I have not yet written that code. Therefore, I'd like to take advantage of the situation to test the timeout case. I have a define...
    on Aug 4, 2009
  • Forum Post: OMAP-L137 EVM - problem with USB Host in linux-2.6.29-rc8-davinci1

    Krzysztof Kanas11924 Krzysztof Kanas11924
    Hi, I am having problems with USB Host functionality on linux-2.6.29-rc8-davinci1 for omap-L137. I use Uboot NFS booting, I am able to download Kernel on omapl (verification is ok I presume) and after run bootm command there is dead silence. The board is not responsive to ping and ssh and on UART2 there...
    on Aug 17, 2009
  • Forum Post: pre built cmem.ko for OMAPL137 in CE 2.23.01

    Sharath Holla Sharath Holla
    Hi all, I wanted to run an application on OMAPL137 board in CE environment. while loading the pre-built cmem.ko, i got following error message. "insmod: error inserting 'cmemk.ko': -1 Invalid module format" I tried building the cmem.ko. Since the MV-Linux package released with...
    on Aug 24, 2009
  • Forum Post: Re: Why OMAP l137 timer does not work

    arthur14426 arthur14426
    Thank u very much , my gel file was modified by others. After I reload the default GEL , problem has been fixed.
    on Aug 26, 2009
  • Forum Post: Adding userland applications in montavista pro Linux 5.0 for use in OMAP L-137 processor

    Haroldo Haroldo
    Hi, I recently bought an OMAP L-137 EVM and have already installed the sdk, configured and written the kernel image to flash and configured an nfs file system. but I haven't been able to configure any of the userland packages that the Montavista distro is supposed to carry , any help on this matter...
    on Aug 26, 2009
  • Forum Post: OMAP L137 McASP slot read issue

    stanley14675 stanley14675
    Hi, We are using TI OMAP-L137 EVM board for one of our application. The Audio expansion slots in the EVM is used for interfacing the Processor to the Front End(FE) board. We are using McASP0 to interface OMAP prosessor to the ADC in the FE board. The ADC we are using is ADS1174 from TI, configured...
    on Sep 1, 2009
12345
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use