• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » OMAP™ Processors » All Tags » boot
Share
OMAP™ Processors
  • Forums
  • Announcements

Browse by Tags

OMAP™ Processors

Welcome to the OMAP™ Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
boot
  • 3530
  • aisgen
  • AM1808
  • ARM Cortex-A8
  • Beagle Board
  • Beagle Board XM
  • beagleboard
  • Beagleboard omap3530
  • bootloader
  • c6748
  • C674x
  • ccs
  • DM3730
  • DSP
  • DSP/BIOS
  • dsplink
  • evm
  • flash
  • jtag
  • kernel
  • L137
  • l138
  • L-138
  • linux
  • Linux Drivers
Related Posts
  • Forum Post: Re: Debug boot firmware

    Bernie Thompson TI Bernie Thompson TI
    Unfortunately the source code to the ROM boot loader is not available (this applies to most other OMAP/Davinci/C6x devices as well). In the case of the OMAP3 the primary source for information on the ROM boot loader is SPRUFD6 , which does not go to the level of entry/exit points but does detail how...
    on Nov 12, 2008
  • Forum Post: Re: Omap-l137 cannot boot by nfs filesys

    BrandonAzbell BrandonAzbell
    YongchaoDeng U-Boot > printenv bootcmd= bootdelay=3 baudrate=115200 ethaddr=00:0e:99:02:f3:c2 nfshost=192.168.0.77 bootargs=console=ttyS2,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock mem=32M stdin=serial stdout=serial stderr=serial ver=U-Boot 1.3.3 (Nov 14 2008...
    on Jan 3, 2009
  • Forum Post: fast SRAM, OMAP-L137

    Flamingo Flamingo
    One of my hardware engineers asks: "We are having variable success getting SRAM. The 166MHz ISSI part seems to be unobtainable right now. There is a 140MHZ ISSI part with some lead time. There is a 133MHZ Micron part that is available. I know if I plug into my PC any speed of RAM the bios...
    on May 12, 2009
  • Forum Post: Re: OMAPL137 SecureDigital versus NAND/NOR Flash?

    Joe Coombs Joe Coombs
    Chikku, When booting from a 16-bit NOR device, you don't need to worry about special EMIFA connections for the initial 8-bit read. Just connect the NOR device to EMIFA (chip select 2) in the standard 16-bit way. The initial read will only look at the lower 8 bits of the first NOR word, but that...
    on May 28, 2009
  • Forum Post: OMAP35x EVM SD boot and bootargs

    WPM WPM
    I am having trouble booting the Mistral EVM board using an SD card. I looked over the existing "booting..." threads but I'm still missing something. For the build machine, I am running VMware 6.52 with Ubuntu 8.04 and CodeSourcery version 2007q3 as the cross compiler. Using the “Getting...
    on May 28, 2009
  • Forum Post: Re: OMAPL137 SecureDigital versus NAND/NOR Flash?

    Joe Coombs Joe Coombs
    Chikku, Sorry, I may have misstated what happens with the first NOR word. The bootloader will read the lowest 8 bits first to determine whether to operate in 8- or 16-bit mode. Then, it will read the rest of the first word before continuing on to the rest of the NOR contents. Also, the wiki page...
    on Jun 11, 2009
  • Forum Post: Android SD Boot on OMAP35x EVM

    mjlyons mjlyons
    I've been trying to get Mistral's Android SD image to boot on my OMAP35x EVM to no avail. I have a Samsung NAND Flash. My boot process: Set SW4 to [1 0 0 1 1 0 0 0] (1 on the left, 8 on the right) Build SD card using "Package1" (pre-generated image) or "Package2" ...
    on Jun 17, 2009
  • Forum Post: Very basic questions concerning linux kernel and file system

    Maik Pflugradt Maik Pflugradt
    Hello, Well, I already spent some hours with my Omap3EVM and the beagleboard but I still do not have a complete overview. I dont know whether this is the right place to post my basic understandings/misunderstandings but I will give it a try anyway. So, what I am actually worrying about are things like...
    on Jul 2, 2009
  • Forum Post: Re: OMAP-L137 Nand Flash support.

    Daniel Allred Daniel Allred
    Misha, Mariana, The boot loader does not implement using a GPIO as the CE for the NAND, and therefore booting from NAND devices that require the CE to be low during the entire tR time is not supported. Regards, Daniel
    on Jul 6, 2009
  • Forum Post: Can't boot after running the Re-flash Procedure - OMAP 35x EVM

    Xi Xi
    Hi, I was trying to re-flash with latest kernel, I operated as guided in the GettingStarted-02.01.01.08.pdf. I did the re-flash several times because it keep respond a "Kernel panic" error after reset. But in my last trying, after I finished the *5.4.2 Running the Re-flash Procedure* ,...
    on Jul 26, 2009
  • Forum Post: 40W output from serial port during 3530 boot

    John F. John F.
    Where does the "40W" text output on the serial console during boot come from? x-loader or from the CPU? Thanks, John
    on Sep 2, 2009
  • Forum Post: OMAP-L137 DSP NOR boot

    Erik Svensson Erik Svensson
    Hello, I have successfully booted the DSP with images up to 32kb from NOR. But we need to be able to boot bigger images so I have been looking into loading images and starting from a first bootloader. My problem is that I don't know how to start the second program. I have this program that should...
    on Oct 21, 2009
  • Forum Post: How to boot the ARM in OMAPL-137 without Linux ?

    liang lee liang lee
    I'm a beginner with OMAPL-137, I'm not familiar with Linux, so I want to use the ARM in OMAPL-137 without Linux. The datasheet just told me to boot the DSP core with D800K001 bootloader, but I don't know how to boot the ARM. Can I boot ARM from NAND? Is there any bootloader tools for ARM...
    on Oct 24, 2009
  • Forum Post: Booting from SPI Flash

    Joe Tijerina Joe Tijerina
    I am using the OMAP-L138 eXperimenter Kit and I'm trying to boot from flash with my kernel and root file system obtained from Timesys Linux. I follow the steps in "GSG:_OMAP-L138_DVEVM_Additional_Procedures" and so far I'm able to copy my kernel and filesystem to flash and set my "bootarg"...
    on Nov 17, 2009
  • Forum Post: SPI0 Flash boot problem.

    Adam10676 Adam10676
    Hi, I can't boot my program from SPI0 Flash onboard EVM memory. Program uses only OMAP-L137 DSP side, DSPBIOS Timer1 , one CLK function, one Task, RS232 460kbs (P1 on EVM). With CCS3.3 in debug or release mode program works correctly. I added code listed below to repleace GEL command: void...
    on Jan 13, 2010
  • Forum Post: Re: Re-Flashing Images to the SPI Flash

    Joe Tijerina Joe Tijerina
    I'm currently having self rebooting issues on my OMAPL138 eXperimenter running Timesys Linux. I had been using the same kernel and RFS, booting with TFTP and NFS, for some time until I started having NFS server issues(separate topic), so as a workaround I am now attempting to boot from the SPI Flash...
    on Feb 17, 2010
  • Forum Post: [OMAP3530] Booting Sequence

    Chris R Chris R
    I want to have a boot sequence on OMAP-3530 that includes UART3, MMC1, and NAND, with NAND the last of the three. SYS.BOOT[5:0] = 0b101111 = 0x2f looks from table 25-4 in spruf98d (3530 Technical Reference Manual) like it would do just fine. However, using my Rev.G OMAP-35x EVM it doesn't seem to...
    on Mar 17, 2010
  • Forum Post: Logic PD OMAP L138 eXperimenters board - u-boot through UART2

    Erik Jones Erik Jones
    I would like to replace the version of u-boot stored in the SPI FLASH with a modified copy. I'm using the DaVinici-PSP-SDK-03.20.00.11 SDK. I am using the OMAP-L138_FlashAndBootUtils_2_25 to generate the AIS file and load it into the SoC per the serial boot instructions. I turn S7:7-8 ON (all...
    on May 10, 2010
  • Forum Post: Re: [OMAPL137] debugging my board through armubl

    Flamingo Flamingo
    Sorry, I didn't see the second question in your post. The majority of the circuitry on our board matches the EVM board that we got over a year ago. I don't have the circuit diagram near me, but I'm guessing that the OMAP has a 300 MHz clock. Did you find the photos from the scope measurements...
    on May 14, 2010
  • Forum Post: OMAPL138 User Boot Loader (UBL)

    Joe Tijerina Joe Tijerina
    My question is regarding the User Bootloader to boot the OMAP L138 SoC from Logic PD's. I have been experimenting with two different UBL. Method 1: Serial Flashing Utility When using the Serial Flashing utility, I use the prebuilt ubl_OMAPL138_SPI_MEM.bin under OMAP-L138/GNU/ubl/ obtained...
    on Jun 4, 2010
  • Forum Post: Questions about OMAP-L138

    Zhang Jingpo Zhang Jingpo
    Dear all: I'm confused with OMAP-L138 these days and still not clear the steps about communication between ARM and DSP. I know it's a big topic to talk about this, but can anyone give answers about the questions below: I have NAND and SPI flash on my own board and L138 can boot Linux from...
    on Jul 13, 2010
  • Forum Post: OMAP-L138 U-boot without UBL / double copy

    Andrea Pastega53856 Andrea Pastega53856
    Hello. We are starting a development over OMAP-L138 . The hardware will boot from SPI-Flash, and will use U-Boot as bootloader and Linux as OS. Starting to experience the Logic development board, I see that the boot sequence consits of a UBL coded in AIS, called by the ARM, that provide to copy...
    on Jul 22, 2010
  • Forum Post: In OMAP-L138, what does DSP core do after boot?

    RY9983 RY9983
    One of my customer does not use Linux. And they do search about OMAP-L138 boot. They know ARM boots first, and sprab41 describes about ARM boot sequence. But, They are wondering about DSP core sequence. When I checked the MDSTAT15 register in OMAP-L138EVM, DSP core was enabled in some boot-mode, and...
    on Aug 4, 2010
  • Forum Post: Re: OMAP-L138: u-boot DRAM layout and personal customization

    Andrea Pastega53856 Andrea Pastega53856
    Hello. Thanks for the help. However my question was different, maybe I have to explain better. I developed a different bootchain, where I use simply an AIS script to setup the hardware and to load U-BOOT in memory, then to execute it. In this way I don't use any UBL. In the AIS of...
    on Aug 26, 2010
  • Forum Post: Re: D800K001 and D800K003 bootloaders

    Louis Dupont Louis Dupont
    Thanks Jeff, I'm using the OMAP L137. I agree that D800K003 is targetted at the DSP. So the DSP will execute the commands dictated by the AIS script. But AISGen for D800K003 now appear to give the option to jump on either the DSP or the ARM next (it wasn't an option with D800K001). So I assume...
    on Sep 2, 2010
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use