• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » C6000 Single Core DSP » C64x Single Core DSP Forum » Interfacing C6414/C6416 to AT91SAM9G54 ARM
Share
C6000 Single Core DSP
  • Forums
  • Announcements
Options
  • Subscribe via RSS

Forums

Interfacing C6414/C6416 to AT91SAM9G54 ARM

This question is answered
rrlagic
Posted by rrlagic
on Apr 06 2012 21:44 PM
Expert1580 points

Hello!

I'd like to ask community advice on the following topic.

We have rather old and fixed digital board with C6414/C6416. On EMIFA we have FPGA, CPLD,  and USB chip. On EMIFB we have 3 parallel flash memory chips of 4MB each. They served as boot source and storage for FPGA images. Because of boot requirements flashes are seen as 8 bit devices, so visible space is 1MB and we use CPLD to produce higher address bits. That solution though proven and works fine is far from elegant. And now we switched to larger FPGA device and run short of flash memory. Somehow we'd like to have more space for DSP and FPGA images and also want to have multiple sets of them. To reload DSP with different program we use two stage bootloader. First stage looks into hardcoded flash memory location for address of primary DSP image. Write to CPLD register is used to create hardware reset strobe to DSP. So this scheme worked pretty well, when we had older smaller FPGA, we could have 2 or 3 images on board, but no more.

So we considering to add ARM controller to that digital board. It will run under some Linux and would have file system on NAND flash. Then ARM could be used to load FPGA chip through SPI port and we free up some space in parallel flashes of the DSP. But then we consider, what if we put all the images on ARM's side? I've heard that booting DSP through HPI is simple and proven process. So we might like to use it. The only concern is that we need more exchange between ARM and DSP. Before we were using USB to connect DSP to the host system. Although USB is kind of host-controller (master-slave) system, we were able to send messages in both directions, from host to DSP and vice versa. Now, when ARM host would be physically present on the board, I wonder, if we can avoid USB at least between ARM and DSP.

Primary requirement is packet exchange with maximum payload of about 256 bytes. We need that both parties can initiate or at least request transfer. Can HPI be used for that purpose? I did not study HPI deeply, I only picked up that it is slave port. Perhaps some GPIO pin can be used to notify ARM host that DSP has something to send. I just guess...

So again, I'd like community comments and advice on this situation.

Thanks in advance.

HPI C64x
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • RandyP
    Posted by RandyP
    on Apr 07 2012 21:08 PM
    Guru61535 points

    My first recommendation is to move to the OMAP-L138 to get an ARM and a DSP in the same chip. Inter-core communication will be a bit easier than using USB or HPI.

    My second recommendation, if you need more fixed-point DSP MIPS than the C674x in the OMAP-L138 can give you, is to look at the C6678 or one of the derivatives with fewer cores.

    Take a look at the Features section at the beginning of either datasheet. You can find out the memory devices they will interface with and the processing power you get.

    Regards,
    RandyP 

    Search for answers, Ask a question, click  Verify  when complete, Help others, Learn more.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • rrlagic
    Posted by rrlagic
    on Apr 07 2012 22:23 PM
    Expert1580 points

    Thanks for your valuable reply.

    We did not settle with OMAP-L138 for the following reasons. First, as you might noticed I did not mentioned any RAM for C6414(6). Applications we are using fit in its L2 memory. OMAP has less on-chip memory, so we would have to add external memory. That's normal way, but would take extra step to verify DDR operation on PCB. Second concern is that C641x @720 MHz or @1 GHz would outperform OMAP in fixed point math. And main concern is that we have several projects on C6414, which we want to be ported with minimal changes.

    As to C66x family, we already set up a project for next platform with C6670. Its my favourite because of its coprocessors. But that power does not come for free. As I understand, C6670 has no memory interface, except for DDR3, though C6678 has EMIF-16. Coprocessing with FPGA is required step, so we are studying the only option to connect C6670 and FPGA - PCIe. Again, to handle housekeeping jobs we want some kind of ARM to run OS and maintain filesystem. So, there should be PCIe switch. This all is doable, just takes time to deal with all these high speed technologies.

    What we are looking now, is some kind of quick solution, which would not change existing PCB and software applications too much. We have proven system with DSP which I described in the first post. We have verified PCB layout and software for mentioned ARM in separate solution. So I wonder if we could merge them.

    As a last resort I consider to change for HPI booting, but preserve USB interface (yeh, that's would be "cool": two processors on the same board would communicate via USB hub on the external interface board), but at least it is well known to us and proven. I wonder, whether HPI can do similar job for us. 

    Have you heard anything about similar solutions?

    Thanks in advance.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Sam Kuzbary
    Posted by Sam Kuzbary
    on Apr 08 2012 08:31 AM
    Expert2655 points

    Greetings,

    Given your state of development, I will recommend the HPI over USB for boot/communication, except it will not port to your next generation based on the 6670.

    Good Luck,

    Sam

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • rrlagic
    Posted by rrlagic
    on Apr 08 2012 09:28 AM
    Expert1580 points

    Sam,

    Thank your for opinion.

    First, HPI definitely won't go to C6670 project as that part has no HPI. As I mentioned, we are considering PCIe both for boot and communications. As soon as evaluation boards and interfaces come, we would prepare prototyping setup.

    As to C6414/C6416, not too many option available. For booting HPI is a best candidate in my opinion. But I have no idea, how to make bidirectional communications over HPI. Could you please elaborate a little on your suggestion? How does DSP send/notify host of data available for transmission? Set couple of GPIO pins for this kind of interrupts?

    Thanks in advance.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Sam Kuzbary
    Posted by Sam Kuzbary
    on Apr 08 2012 09:52 AM
    Verified Answer
    Verified by rrlagic
    Expert2655 points

    Greetings,

    For the C6670 to boot and operate over PCIe, I think there is still a need for a secondary boot loader beyond internal ROM to help setup PCIe for such.  Good luck with that.

    For C641x, using HPI for boot is no brainer.

    If a simple non/queueing interface suffice, then once your app is up, you can have a static area in your memory to use for a command register (from Host to DSP), a response register (from DSP to Host), and a buffer[x] of certain size x to use if the command or response do have a body. 

    In your app, a timer ISR (with or without DSP/BIOS) or a general loop, can be used to manage a simple but robust exchange between your Host and DSP.  You can design it in any way fit for a Host-Master/DSP-Slave.

    If an advanced queueing interface is required, you can then built it using DSP/BIOS and the HPI interface Host-to-DSP and DSP-to Host interrupts

    I hope this help.

    Sam

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • rrlagic
    Posted by rrlagic
    on Apr 08 2012 21:11 PM
    Expert1580 points

    Sam,

    Thanks again.

    With your hint I picked, that host can interrupt DSP by write to control register, and DSP can interrupt host by setting HINT signal. Thus, no extra connections required to make bidirectional interrupt signalling.

    As I understand, we have to develop kind of low level driver, which would serve as transport instead of existing USB driver. As you mentioned, there should be some static buffers for commands and responses, whose absolute location is known to the host. Then to issue a command the host performs HPI writes to command buffer according to HPI sequence and sets Host-to-DSP interrupt to let DSP application know about ingress command. If DSP has response to host, it first prepares response in response buffer and sets HINT interrupt to the host. Host catches the interrupt and performs HPI read from response buffer.

    Am I missing something?

    Just in case, if TI's people may have some example code, could you please share that too?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Sam Kuzbary
    Posted by Sam Kuzbary
    on Apr 09 2012 07:46 AM
    Expert2655 points

    Greetings,

    You got the idea.  Now you can poll these command/response registers and do away without host-to-dsp or dsp-to-host interrupts if the traffic throughput is low, and no queueing of many host reqs or dsp reqs.

    If no example code form TI, and you want to go this way, we may take this offline, and you can send me your e-mail so that I can throw at you some example code.

    Good Luck,

    Sam

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • rrlagic
    Posted by rrlagic
    on Apr 10 2012 20:51 PM
    Expert1580 points

    Sam,

    Thank you for sharing opinion. If you don't mind to share some code, please send to "my forum nickname" at google.com.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Sam Kuzbary
    Posted by Sam Kuzbary
    on Apr 11 2012 08:42 AM
    Expert2655 points

    Greetings,

    Test e-mail to rrlagic@google.com bounced back.

    Sam

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use