I am using DM6437 EVM, NDK version 2.0.0 and client.pjt example.

By chance I found this problem:

1. I connect directly my EVM and my PC

2. I configure my Windows PC with static IP address:
   IP address: 10.13.13.11
   NetMask: 255.255.0.0

3. I configure in the C code of client.pjt example a static IP address:
   IP address: 10.13.0.87
   NetMask: 255.255.255.0

4. I try to ping the EVM from my PC and I am able to ping it,
   but not always.

In my opinion this behaviour is not expected: the EVM should answer only
to a ping from an address 10.13.0.x because its net-mask is
255.255.255.0, instead sometimes (but not always) it answers to 10.13.13.11.

If I replace my EVM with another PC (Static IP address: 10.13.0.87,
NetMask: 255.255.255.0), I have the correct behaviour, in fact 10.13.0.87
doesn't answer to pings from 10.13.13.11.

Have you ever seen this behaviour? Is it an NDK problem or is it a configuration
problem? Have you already solved it?

Thank you very much!

Umberto Amadei