• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » C6000 Single Core DSP » C64x Single Core DSP Forum » Wrong DSP Internal Clock Speed
Share
C6000 Single Core DSP
  • Forums
  • Announcements
Options
  • Subscribe via RSS

Wrong DSP Internal Clock Speed

Wrong DSP Internal Clock Speed

This question is answered
Nuno Pereira
Posted by Nuno Pereira
on Jul 22 2011 05:25 AM
Prodigy160 points

Hello to All

I have some doubts about the internal clock speed of DSP programming.

The original program that is running in one of my company boards uses a TMS320C6413-500 and it was not written by me.

This DSP configures the PLL using input ports and in this board we are using a 50 Mhz clock with a x10 multiplier.

I check the internal PLL registers of the DSP and everthing seems ok, at least the x10 value is correctly assigned in the DSP register

I am making small modifications in this code, but since I waiting for the emulador, I am testing the performance of the code using GPIO ports and a logic analyzer.

I notice, that a small GPIO logic switch between 0 and 1 and then return to 0 takes about 60 ns seconds.

The Code is the first thing that I execute in the program, but I also test it in the middle of the code.

I define new macros also shown bellow to speed up the logic switch, but I intend to use the orignal ones in the CSL library, but the original ones take more than 200 ns

Bellow is the code that I am using to access the GPIO 0 and 3

hGpio = GPIO_open(GPIO_DEV0,GPIO_OPEN_RESET);

GPIO_configArgs(hGpio,

GPGC_GP0_3, // gpgc Global control register value

GPEN_GP0_3, // gpen GPIO Enable register value

GPDIR_GP0_3, // gpdir GPIO Direction register value

GPVAL_GP0_3, // gpval GPIO Value register value

GPHM_GP0_3, // gphm GPIO High Mask register value

GPLM_GP0_3, // gplm GPIO Low Mask register value

GPPOL_GP0_3 // gppol GPIO Interrupt Polarity register value

);

GPIO_pinEnable(hGpio,GPIO_PIN0 | GPIO_PIN3); // old DMA0/1

// from here

GPIO_pinSet(GPIO_PIN0);

GPIO_pinSet(GPIO_PIN3);

error = 1; // dummy code to avoid compile to optimize code and remove the switch from 0 -> 1 -> 0

GPIO_pinReset(GPIO_PIN3);

GPIO_pinReset(GPIO_PIN0);

// to here = 60ns

The macros above are defined as

 #define GPIO_pinSet(Pin) *((UINT32 *) 0x01B00008) |= Pin

#define

GPIO_pinReset(Pin) *((UINT32 *) 0x01B00008) &= ~Pin

 

 

If the clock was running at 50 MHZ with instruction cycle of 20 ns, 60 ns to do these instrunctions could be fare, but at 2ns per instrunction is difficult to me to believe that it takes 30 instructions to switch from 0->1->0

best regards

Nuno

 

 

 

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Brad Griffis
    Posted by Brad Griffis
    on Jul 22 2011 15:05 PM
    Guru57330 points

    This test is a poor indicator of DSP clock speed for 2 reasons:

    1. The IO cells are not designed for toggling faster than 12.5 MHz.
    2. Even toggling at 12.5 MHz is not possible because the configuration bus where the GPIO registers reside is very slow.  It takes many cycles to perform an access to configuration space.

    Here's a snippet from the data sheet which mentions these things:

    If you want to know the clock speed, why not simply look at CLKOUT4 or CLKOUT6 on a scope?  That's the best way to know the speed...

    ---------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------- 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Nuno Pereira
    Posted by Nuno Pereira
    on Jul 25 2011 08:46 AM
    Prodigy160 points

    Hello Brad

    Thanks a lot for your response. Based on your response I can assume that, the switching time is not constant and it may differ depending the internal state, so I cannot use it for timing control.

    Basically I would like to have a good mechanism to control the speed of some blocks of the code, and since this GPIO pins were available ...

    The application of the board is time critical, and it must performe all the calculations in less then 2uS, for each fw cycle.

    I try to profile the code, but since the parameter -O2 of the compiler is used, I was not able to trace the number of cycles of each block in the code.

    I am using CCS 4.

    Can you suggest a way to make more precise calculations regarding time inside the fw? Perhaps using other pins?

    Regarding your idea, I do not have these 2 pins available in my mictor connectors, so it is dificult to me to measure these pins.

    I look at schematics, and it seems to be a test point for CLKOUT4. I will check this on the board

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Brad Griffis
    Posted by Brad Griffis
    on Jul 25 2011 09:11 AM
    Guru57330 points
    6416 benchmark framework.zip

    Nuno Pereira

    Basically I would like to have a good mechanism to control the speed of some blocks of the code, and since this GPIO pins were available ...

    How about using a timer?

     

    Nuno Pereira

    Can you suggest a way to make more precise calculations regarding time inside the fw? Perhaps using other pins?

     I'm attaching some code I wrote a really long time ago which uses a timer to determine how many cycles a function takes.  It was written for c6416 but should be pretty close to what you're doing.  You can get rid of the cache invalidation code if you like.  In other words, invalidating the cache will hurt your performance.  I was trying to get a "cold cache" benchmark but of course performance will improve if something is cached.

    ---------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------- 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Nuno Pereira
    Posted by Nuno Pereira
    on Jul 28 2011 06:14 AM
    Prodigy160 points

    Hi Brad

    I check your source code and I realize that must of the work I already have available in my own project.

    I also have a timer running, so I decide to create a macro to measure the difference between a certain read of the timer count with a next read a few instructions later.

    Meanwhile, I manage to program clkout4 output and check the HW in a test point to confirm that the DSP is running at 500MHz.

    Now I have two issues to undserstand.

    1 - If I made a reading like "Init = TIMER_RGET(CNT2)" and then put a dummy instruction in the middle and calculate the diference between the new timer counter like "TIMER_RGET(CNT2) - Init", I realize that the diference is a number like 16. Since the timer clock is divided by 8, this means that the DSP takes about 16 x 8 x 2ns to execute the code between the readings. I think this value is huge. Any Ideas?

    I do not "printf" the value, since "printf" will delay a lot my code, so I basically write the value in the memory space and read it later.

    2 - My code does not have any interrupt programmed, and each time that I read a complete cycle of the main loop I get values like 0x5A to the number of timer counts.

    If I change the macro to give me the maximum value using _max2, between the current value in memory and the new timer counts, I get values like 0x203.

    I notice that this increase of counts, just happen after a EDMA transfer, and if I put the init counter value a few instructions after the EDMA transfer, the values are again near 0x5A, but If I put it, just after the CIPRL check bit instruction, the values goes up to 0x203.

    This do not happen in all the cycles, because even in this condition if I remove the _max2 primitive, the values are again near 0x5A, meaning that it just happens a few times, because I cannot get any 0x203. Any Ideas how to grab this abnormal increase of counts?

    best regards

    Nuno Pereira

     

     

     

     

     

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Brad Griffis
    Posted by Brad Griffis
    on Jul 28 2011 07:21 AM
    Verified Answer
    Verified by Nuno Pereira
    Guru57330 points

    Accesses to "configuration space", i.e. any peripheral registers, will be very slow in general.  That's why you see such a large count with only a single instruction between timer reads.  In other words, the timer reads themselves are taking a number of instructions.  There are some limits to the precision with this method.  You can improve the accuracy a bit by figuring out the overhead of the benchmark itself by doing a couple timer reads with zero instructions in between.  You can subtract that number from all subsequent readings (or just keep it in mind at least).

    I would guess that accesses to the configuration bus are also responsible for the increase in counts related to EDMA activity.  Interrupt overhead is another thing I would generally consider though you said you don't have any interrupts enabled.

    ---------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------- 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • David Watson
    Posted by David Watson
    on Nov 24 2011 07:48 AM
    Prodigy150 points

    Hi guys

    Sorry to hijack this thread, but see when using Brad's timer code, I take it if you divide the result of the timer code by the clock speed of the processor, then that will give you the execution time of your code in seconds? Sound right?

    Cheers

    David

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Nuno Pereira
    Posted by Nuno Pereira
    on Nov 24 2011 08:15 AM
    Prodigy160 points

    Hello David

    The problem that I was facing, appears because I am trying to measurer DSP performance for a very short period of instructions, meaning values around a couple of hundreds nanosecs and not seconds.

    The problem is that by accessing TIMER registers, the instruction itself take a lot of time, because I believe that this can be called a slow register for the DSP internally.

    To avoid all of this, I am currently using another process the measure DSP performance, that works in my case.

    I start to use QDMA. With QDMA you can simulate a write to a destination address that will generate a CS in unused memory block.

    With an oscilloscope or data analyzer I was able to measure the time between two CS and have a highly accurate value.

    You can initialy set up all the values for one trigger QDMA transfer and then, every time you want to measure something, just trigger a new dummy QDMA at the begging of the code and another at the end.

    It works quite nice for me :)

    best regards

    Nuno Pereira

     

     

     

     

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • David Watson
    Posted by David Watson
    on Nov 24 2011 09:13 AM
    Prodigy150 points

    Hi Nuno

    Thanks for getting back to me. I'm not using the QDMA of the DSP, I was just looking for a quick way to time my code and I came across this thread. Do you know if I divide the cycles by the CPU clock I will get the time in seconds for the code to execute?

    Thanks for your help

    David

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Nuno Pereira
    Posted by Nuno Pereira
    on Nov 24 2011 10:03 AM
    Prodigy160 points

    Hi David

    You have to take in consideration the type of DSP you are using

    In my case, since I use a 500MHz clock each instruction takes 2ns, but the clock tick is divided by 8 (you can check in the datasheet, waht is your case), meaning that the value that you get by reading the CNT register must be multipled by 2ns x 8 = 16ns.

    best regards

    Nuno Pereira

     

     

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • David Watson
    Posted by David Watson
    on Nov 24 2011 10:13 AM
    Prodigy150 points

    Hi Nuno

    I'm using the C6416T which runs at 1GHz with the tick divided by 8. So does that mean I multiple the result by 8 (to get cycles) and then divide by 1x10^9 to get seconds? So for example, the cycles I got from the timer for my code execution was 5926880 (after being multiplied by 8). So I multiply this by 1x10^-9 to get the time in seconds? Which was 0.0474 seconds. Do you agree?

    Thanks for your help

    David

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Brad Griffis
    Posted by Brad Griffis
    on Nov 24 2011 10:40 AM
    Guru57330 points

    I agree. Timer cycles x8 is CPU cycles (for 6416). CPU cycles times cpu period gives seconds

    ---------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------- 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Nuno Pereira
    Posted by Nuno Pereira
    on Nov 24 2011 10:44 AM
    Prodigy160 points

    Hi David & Brad

    I also agree, but watch out for timer overlaps. You must set the PRD register to a period time with a value big enough to avoid overlaps, otherwsie the value that you are reading can be only a fraction of your time.

    best regards

    Nuno Pereira

     

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • David Watson
    Posted by David Watson
    on Nov 24 2011 11:32 AM
    Prodigy150 points

    Hi Nuno and Brad

    Thanks for getting back to me. I'm a bit of a noob when it come to timers so I was just using the setup contained in the code Brad posted. Do you know if that setup is ok and will not result in any overlap?

    Thanks again

    David

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Brad Griffis
    Posted by Brad Griffis
    on Nov 24 2011 12:07 PM
    Guru57330 points

    My code maxes out the period.  You would have to run for more than one minute to overflow.  I think it would be quite obvious.

    If you have many functions that you're benchmarking you might want to tweak the way the code works.  Currently the code zeros out the timer and starts it running from 0 at the start of the benchmark.  If you wanted to instead benchmark many functions you might instead want to simply leave it running all the time and simply do a difference of the time stamp at the start and end of the function you're benchmarking.

    ---------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------- 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • David Watson
    Posted by David Watson
    on Nov 24 2011 12:14 PM
    Prodigy150 points

    I only have the one function I'm benchmarking and I call the start and stop before and after respectively. By maxing out the period do you mean it gives the shortest period and therefore the greatest accuracy?

    Cheers

    David

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use