hello:
I am use the NDK 1.93 in c6455, C6455 is as a server, and the client runs in PC, I can make sure the client is right, But when the client connets the c6455 server, I find sometimes server accept success, sometimes the server accept failed! When failed,The accept() function does not return amd I ping the server,it is OK! But telet the port is not successful.I wonder if heap or stack have influence , so I increase the heap to 512KB and stack to 128KB, But it does not change! I have two threads, one for recv ,and the other is for send. Both send and recv thread have the same port! I Need Help !
Thanks!
if you are in China beijing,please contact me. weizhiheng99@yahoo.com.cn
I have use NDK for 6455 for about 5 years.
Si Cheng and Zhiheng Wei,
For the benefit of the E2E Community, please at least post a description of the problem as you have found it and a description of the solution that you have found. With this information, others like Si Cheng will find answers by searching the forum. And Zhiheng Wei's words will help all of those people.
Regards,RandyP
Search for answers, Ask a question, click Verify when complete, Help others, Learn more.