Hey,
I am trying to configure an EDMA transfer through EMIFA. I have configured 2 channels i.e. 54 and 55 for gpio 6 and gpio 7 event triggers. My EDMA interrupt is working properly. Now i want glow an LED i.e. make gpio pin 14 and 15 high in the ISR. I am trying to bind the ISR statically through .tcf file.
I read the wiki page on how to configure the interrupts through BIOS, but it isn't working. Could you please how to go about it. Attached the project in .rar file. Kindly help.
I have used Mask-able interrupt 4 for binding the ISR. The same can be seen in the .tcf file also.
Additionally, i am facing another problem. The EDMA registers .i.e OPT,SRC etc, which are the part of PaRAM set gets reset when the EDMA event occurs, and i have to recall the setup every time an event occurs. I believe this is not the right way to go about it. Can you please tel me how i can prevent my PaRAM set registers from resetting?
Regards
Akshay