Hello,
There are two McBSP 0 and 1 in DM6437 EVM.
I would like to do McBSP 0 as transmitter and McBSP1 as receiver and want to do data transfer between them.
My Questions is
Is it possible to configure McBSP0 as transmitter and McBSP1 as receiver and data can be transmit between them?
if yes, is there any external pin connections are required on EVM board?
Regards,
Nares