How can I do this, is there any examples or recommendations to connect to a WiFi network DM6437
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How can I do this, is there any examples or recommendations to connect to a WiFi network DM6437
Hi Ruslan,
Thanks for your post.
If EVM is connected to a wifi based PC, then, yes it is possible. but Sorry, TI does not support any example software or drivers to demonstrate it.
Maybe, you could also refer the below E2E post to set up wifi router with DM6437:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/t/104217.aspx
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/t/7012.aspx
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------