hello to all
I want to use NOR FALSH Boot in 6748(evmc6748). I use AISgen_d800k008.exe in coverting .out file to .bin file. In AISgen_d800k008 configration,the PLL1,PLL0,SDRAM,the boot mode chose SPI1 FLASH.
When I assign .data and .far section to DDR. . The bin file can not auto boot after the bin file flashed to the NOR FALSH.
When I assign .data and .far section to IRAM. The bin file can auto boot after the bin file flashed to the NOR FALSH.
How can I auto boot successful when I assign .data and .far section to DDR? Or when I assign .data and .far section to DDR, whether the bin file can boot start from NOR FLASH?
THANKS