Hello,
I used NDK ver 2.0.0 on my c6455 custom board. It was ok with 10/100 FullDuplex communication but when i change configuration of c6455 into "GMII" the interface between board and PC is unreachable!
this message has been shown on CCS v5.2.1 :
[C64XP_0] TCP/IP Stack Example Client
[C64XP_0] Using MAC Address: e7-11-13-08-7c-45
[C64XP_0] EMAC should be up and running
[C64XP_0] EMAC has been started successfully
[C64XP_0] Registeration of the EMAC Successful
[C64XP_0] Network Added: If-1:xxx.xxx.1.2
[C64XP_0] Service Status: Telnet : Enabled : : 000
[C64XP_0] Service Status: HTTP : Enabled : : 000
[C64XP_0] Link Status: 1000Mb/s Full Duplex on PHY 7
and my PC recognizes this 1Gb/s local network, too.
Then I ping but no interface exist!
Should I change any code in NDK or any consideration is there here?