Hello:
I built my project sum=a+b where a=3 and b=4. Then I printed sum out with print function.
I literally did not write any cmd file to allocate the memory. But why the console could show the result "sum=7" as same as VS2010 C programming?
The C code at CCS is essentially runnning on my DSK. Hence using the memory to store my three variables a b and sum should be required. But why it worked without cmd file? Did they even never used the memory or register of my DSK?
I cannot distinguish when should I write cmd file to allocate memory and when I do not write cmd file which is simliar to VS2010?
Thanks