I interfaced a DSP (TMS320C6424) with a Freescale CPU (MPC8313E) using the 32 bit PCI Interface.
There is actually no problem. Everything work perfectly fine. I probed some signals on the PCI interface to check the signal quality and the signals are mostly very badly shaped: Down to -1.05V undershoot and up to +4.24V overshoot. It certainly don't respect the absolute maximum rating.
I did not use any serial resistors on the PCI signals as everybody seams to say that they are not required. There are not many examples of using the parallel PCI bus and some are contradictory.
The nets are about 4 inches long with impedance controlled to 50 ohms +/- 10%. The MPC8313 is configured as PCI master and the C6424 as PCI slave. I think that +4.24V overshoot may be harmful for the internal PCI clamping diode and some precautions need to be considered. A 33 ohms series resistors may be required, at least on one of the devices (The TMS320 or the MPC8313), or maybe on both.
I may like to have your opinion about it.