1.Commnunication between 2 C6455 chips with UDP protocol
Supposing that the C6455 called A is the transfer and the B is the receiver. After the initialization of A and B, B runs the rcvfrom function and then A runs sendto function. In normal condition,B should receive packages that come from A,but we found B received nothing. Therefor, B gets the data packages from A when A running rcvfrom function. Is this right? If not, can you explain to us what's wrong in the communication?
2.Commnunication between 3 C6455 chips with UDP protocol
Supposing that the C6455s called A and B are transfer, and C is receiver. A and B send data packages to C at the same time.And finally we found the communication between A and C is normal ,but B and C is abnormal. Does C6455 support the communication that A and B send data packages to C at the same time?if does,what's the problem in the communication we may meet?And can you give us some advice that could look for what's wrong has happend in our communication?