Hello,
How SIMILAR FUNCTIONALITY is between the C6745 and the C6748 (NOT the C6742). If one starts with the C6748 Evaluation design and put in a C6745, how much trouble will they have getting the DSP peripherals configured and the I/O devices and device drivers in the StarterWare to work. I realize the pinouts between the C6745 and C6748 are different but hoping the hardware pin names and functionality are the same for the peripherals supported by both devices. Specificaly the EMAC, USB, and SDRAM.
Thanks,
Mehrdad.