I am using edma3_lld_02_11_13_17 to do dma tests for OMAP L138 and i built stand alone application by reading the EDMA3_LLD guide. I have used XDC xdctools_3_31_02_38_core and BIOS bios_6_42_01_20 and CCS c6000_7.4.12. I was able to build and when I loaded the edma3_drv_omapl138_sample_c6xdsp_debug.x674
But when I load , I dont have trace0 file created.
The output is
remoteproc0: dsp is available
remoteproc0: Note: remoteproc is still under development and considered experimental.
remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
remoteproc0: Unsupported class: 28
NET: Registered protocol family 40
and
cat: can't open '/debug/remoteproc/remoteproc0/trace0': No such file or directory